If you click the print icon (
) while a popup is active, the printer prints
the popup text over the existing topic text. Use the following procedure
to print the popup text separately.
Activate the popup.
Move the cursor over the popup text.
Right-click.
If the popup closes, reopen it and make sure that the cursor is over the popup when you right-click.
From the menu that appears, choose .