Real Time

Configuring a Crossover LAN for a PXB Connected to a PC

To set up your system for a crossover LAN connection (direct connection between a PC and a PXB, or PXB to other instruments), do the following:

Configure the PXB 

  1. From the Control Panel (located in the XP Start menu), double-click Network Connections.

  2. Right-click Local Area Connection and select Properties.

  3. In the Local Area Connection Properties dialog box, highlight Internet Protocol (TCP/IP). Ensure that the checkbox remains checked.

  4. Click Properties.

  5. Select Use the following IP address (radio selection).

  6. Enter the IP address:

  7. Click the Subnet mask entry field; an address appears.

  8. Click OK to accept the configuration.

  9. Close the Local Area Connection Properties dialog box.

  10. Close the Network Connections window.

To Reconfigure for a LAN Connection

  1. Connect the LAN cable.

  2. From your PXB's Control Panel, click Network Connections.

  3. Right-click Local Area Connection and select Properties.

  4. In the Local Area Connection Status dialog box, click Properties.

  5. In the Local Area Connection Properties dialog box, highlight Internet Protocol (TCP/IP). Ensure that the checkbox remains checked.

  6. Click Properties.

  7. Select the Obtain an IP address automatically option or enter your system IP address.

  8. Click OK to accept the configuration.

  9. Close the Local Area Connection Properties dialog box.

  10. Close the Local Area Connection Status dialog box and the Network Connections window.