Real Time

Preferences Dialog Box

To open the Preferences dialog box, click View > Preference in the Signal Studio menu bar.

Double-click a carrier in the Preferences dialog box to toggle the state of the carrier off or on or use the drop-down menu and select Off or On. When the carrier state is set to On, the carrier appears in the Closedlist of carriers shown when you click the Add Carrier button in the Waveform Setup node or the Carrier node. When the carrier state is set to Off, it does not appear in the list. The figure below shows the default settings for the Carrier Aggregation n node. (You can only have one LTE-A Aggregate Carrier playing at a time.)