DMRS Slot Settings

Refer to General Settings.

LTE FDD Configuration Summary Table

This section defines the LTE/LTE-Advanced FDD DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the LTE FDDn Uplink's tree nodes.

Restores all of the LTE/LTE-Advanced FDD channel's parameters to their default conditions.

DMRS Slot Settings

These values are active for each slot when the Parameter Calculation Mode is set to Manual.

DMRS Seq Index

Range: 0 when RB ≤ to 5, 0 or 1 when RB > 5

Default: 0

Enter a value for the sequence index for the demodulation reference signal in each slot of the subframe. This value is used when Parameter Calculation Mode is set to "Manual". Refer to 3GPP TS 36.211.

DMRS Grp Index

Range: 0 to 29

Default: 0

Enter a value for the group index for the demodulation reference signal in each slot of the subframe (See 3GPP TS 36.211). Sequence groups are typically used to multiplex reference signals in neighboring cells. This value is used when Parameter Calculation Mode is set to "Manual".

DMRS Cyc Shift

Range: 0 to 11, step 1

Default: 0

Enter a value for the cyclic shift for the demodulation reference signal in each slot of the subframe (See 3GPP TS 36.211). Cyclic shifts are used to multiplex reference signals from different terminals within a cell. This value is used when Parameter Calculation Mode is set to "Manual".