The PUSCH transmission is controlled based on the HARQ packet number.
Refer to General Settings.
This section defines the LTE/LTE-Advanced FDD DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the LTE FDDn Uplink's tree nodes.
|
Restores all of the LTE/LTE-Advanced FDD channel's parameters to their default conditions. |
Choices: All Processes On | Customize
Double click or use the drop-down menu to set the state of the transmission control based on HARQ process number.
|
All Processes On |
Each state of Process [n] is on. |
|
Customize |
Each state of Process [n] can be configured to on or off. |
The number of HARQ processes is fixed at 8.
Choices: On | Off
Double-click of use the drop-down menu to turn the state of the UL-SCH HARQ process state On or Off when the Process Transmission Control is set to Customize. The PUSCH state together with the process settings control the transmission of the
Figure 1. Example of PUSCH assignment with Process Number#0 enabled