Uplink_(LTE-A TDD PRACH)

Click the Wizard button to access a dialog box from which you can configure the PRACH Preamble. Click the links in the table below for parameter definitions.

1. Cell Parameters

2. PRACH Parameters

State

PRACH Configuration Index

Antenna Port

PRACH Preamble Auto-Calculate

Total number of Antennas

 

PRACH DFT Swap

 

1. Cell Parameters

State

Double-click or use the drop-down menu to turn the uplink transmission off or on.

Antenna Port

Displays the antenna port number.

Total number of Antennas

Displays the total number of antennas.

PRACH DFT Swap

Choice: Off | On

Default: Off

Double-click or use the drop-down menu to turn PRACH DFT Swap on or off.

PRACH DFT Swap influences how data is mapped to resource elements in the physical uplink shared channel after discrete Fourier transform is performed. PRACH DFT Swap can be turned on or off to provide two different interpretations of how data should be mapped to resource elements in PUSCH channels.

2. PRACH Parameters

PRACH Configuration Index

Range: 0 to 63

Default: 0

Enter a value for the PRACH Configuration Index.

PRACH Preamble Auto-Calculate

Choice: Off | On

Default: Off

Double-click or use the drop-down menu to turn PRACH Preamble Auto Calculate State on or off.

If the state is on, the sequence will be automatic selected by the preamble index. If the State is offset, the sequence can be manually selected by logic root sequence index and cyclic shift v.