The radio format and configuration displayed depend on the selected
carriers. Settings under Categories 1, 2, and 3 apply to all basic and
advanced carriers. The fading parameters in Category 4 are available for
Advanced LTE TDD carriers only.
This table enables you to view the key parameters for each carrier in the waveform. Double-click a carrier row to activate the setup tables for that carrier.
You can also add or delete carriers using the buttons above the table. (Older carrier configurations display the icon without the button name.)
An asterisk following a carrier entry indicates that parameters for the carrier have changed.
Click this button to open a window with pre-defined carrier configuration selections. Double-clicking a configuration replaces the current configuration in the setup table.
Click this button to open a drop down list from which you can select a carrier to add to the setup table. The carrier is inserted above the currently selected carrier in the table. The maximum number of carriers is 16.
You can also make older carrier versions available by clicking View > Show Legacy Carrier from the menu bar.
Click this button to delete the currently selected carriers in the setup table. You can highlight multiple carriers by holding down the CTRL key while selecting the carriers. You can also use the SHIFT key to select a succession (group) of carriers.
Click this button to quickly add a copy of the selected carrier to the carrier configuration summary table.