The software does not use these settings when it is controlling multiple instruments as shown in the tree view.
|
1. Timing Adjustment Settings |
|---|
|
|
This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. When using multiple instruments as shown in the tree view, this button is not displayed. |
|
|
This button displays in place of the Settings Current button. It indicates that the instrument settings are not currrent and need to be updated with the new software settings. Click this button to update the insturment's settings. This button shows in all windows regardless of where the change was made. When using multiple instruments as shown in the tree view, this button is not displayed. |
Choice: Off | On
Default: Off
Coupling: This setting is inactive and set to off when using multiple instruments as shown in the tree view.
Double-click or use the drop-down menu to turn Timing Adjustment State on or off. If the Timing Adjustment Control State is enabled, the timing adjustment control of the Physical Channels is activated.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:TADJust:STATe 1|0|ON|OFF
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:TADJust:STATe?
Range: 3 to 14
Default: 6
This parameter is displayed when the Time Adjustment Control State is On. Enter a value to set the delay from the Timing Adjustment feedback signal timing to the data generation timing. The unit of the delay number is subframe.
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:TADJust:EXTernal:DATA[:SERial]:DELay <val>
[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:TADJust:EXTernal:DATA[:SERial]:DELay?