Installation Steps: 1 2 3 4 5 6 7
Some instruments require unique configurations for use with Signal Studio and are not described in this topic. In these cases, refer to Tutorials for specific information on how to configure your instrument.
Ensure the signal generator is turned off.
Connect the signal generator to the computer using one of the following methods for instrument control:
LAN
Network — connect
both the signal generator and the computer to an external LAN network
using standard LAN cables.
Crossover
LAN — connect
the signal generator directly to the computer using a crossover LAN cable.
(You will need to configure
your PC.)
GPIB
— connect
the signal generator directly to the computer using a GPIB cable.
This section only applies if you are connecting a PC to the PXB. If you are using the PXB as the controller, no connections are required and you can ignore this section.
Ensure the PXB is turned off.
Connect the PXB to the computer using one of the following methods for instrument control. See the PXB's online documentation for GPIB and LAN configuration information.
LAN Network —
connect
both the PXB and the computer to an external LAN network using standard
LAN cables.
Crossover LAN —
connect
the PXB directly to the computer using a crossover LAN. (You will need
to configure your PC
and the PXB.)
GPIB — connect the PXB directly to the computer using a GPIB cable.