Real Time

Configure UCI Window (Basic LTE-A TDD Uplink)

Before adding a UCI channel as described below, delete any existing transport channel, physical channel, or resource block group that occupies the resource blocks that your new UCI channel will occupy. If you add a new UCI channel without first deleting a conflicting channel or resource block group, a "code conflicted" error occurs when you generate the waveform.

The physical uplink control channel, UCI, carries uplink control information. The UCI is never transmitted simultaneously with the PUSCH from the same UE. For frame structure type 2, the UCI is not transmitted in the UpPTS field.

The physical uplink control channel supports multiple formats as shown in Table 1. Formats 2a and 2b are supported for normal cyclic prefix only.

Table 1. Supported PUCCH formats

PUCCH Format

SRS Support

Modulation

1

x

n/a

1a

x

BPSK

1b

x

QPSK

2*

n/a

QPSK

2a*

n/a

QPSK + BPSK

2b

n/a

QPSK + QPSK

3 x QPSK

*Applicable for Normal cyclic prefix only.

All PUCCH formats use a cyclic shift of a sequence in each symbol, where is used to derive the cyclic shift for the different UCI formats. The quantity varies with the symbol number l and the slot number n according to

                                                        

where the pseudo-random sequence generator shall be initialized with at the beginning of each radio frame.

The physical resources used for UCI depends on two parameters, and , given by higher layers. The variable denotes the bandwidth in terms of resource blocks that are reserved exclusively for UCI formats 2/2a/2b transmission in each slot. The variable denotes the number of cyclic shift used for UCI formats 1/1a/1b in a resource block used for a mix of formats 1/1a/1b and 2/2a/2b. The value of is an integer multiple of within the range of {0, 1, …;, 8}, where is defined in section 5.4.1. No mixed resource block is present if . At most one resource block in each slot supports a mix of formats 1/1a/1b and 2/2a/2b. Resources used for transmission of UCI format 1/1a/1b and 2/2a/2b are represented by the non-negative indices and , respectively.    

Click the Add New Channel button in the Transport Channel node and select UCI to open the Configure UCI window. Figure 1 shows the Configure UCI window with the default settings.

Figure 1. UCI with Default Settings

Format

Choice: 1 | 1a | 1b | 2 | 2a | 2b |3

Default: 1

Enter a format number for the PUCCH. The modulation type and number of bits per subframe for each format is shown in Table 1 above.

Refer to 3GPP TS 36.211, 36.212 and 36.213.

Modulation Type

Displays the modulation type for the PUCCH for the selected format as shown in the table above.

Refer to 3GPP TS 36.211, 36.212 and 36.213.

Subframe Number

Enter the number(s) of the subframe(s) that the UL-SCH will occupy. You can enter the number of a single subframe, two or more subframes separated by commas, or a range of subframes (for example, 1-3)

N_RB(2)

Range: 0 to (Max Resource Block – 1)

Default: 1

Enter a value for the UCI N_RB(2) number.

N_CS(1)

Range: 0 to 8

Default: 0

Enter a value for the UCI N_CS(1) number.

nPUCCH(1)

Range: 0 to minimum (2047 or Calculated Maximum Value).

Calculated Maximum Value will vary with the related PUCCH settings.

Default: 0

Enter a value for the UCI nPUCCH(1) number. Specifies the resource index for PUCCH formats 1/1a/1b.

Calculated maximum value means the resource is at the center of the system bandwidth.

A resource used for transmission of a PUCCH format 1/1a/1b is represented by the non-negative indices .

This is one of the values used for generating and mapping PUCCH (see 3GPP TS 36.211, 36.212, and 36.213).

nPUCCH(2)

Range: 0 to Calculated Value

Calculated Value will vary with the related PUCCH settings.

Default: 0

Enter a value for the UCI nPUCCH(2) number.

A resource used for transmission of a PUCCH format 2/2a/2b is represented by the non-negative indices

This is one of the values used for generating and mapping PUCCH (see 3GPP TS 36.211, 36.212, and 36.213).

nPUCCH(3)

Range: 0 to (Number of RB in the system bandwidth) * 5 – 1

Default: 0

Specifies the resource index for PUCCH format 3.

Refer to 3GPP TS 36.211, 36.212 and 36.213.

Delta Shift

Range: 1 to 3

Default: 1

Enter a delta shift value which is used to calculate the cyclic shift alpha for the UCI.

Resource Blocks

Displays the numbers of the resource blocks occupied by the UCI, separated by a comma. If you change the mapping area size, mapping area offset, or first resource block number, the resource block numbers are updated accordingly when you click in this cell.

Group/Sequence Hopping

Choice: Off | Group Hopping | Sequence Hopping

Default: Off

Double-click or use the drop-down menu to enable the hopping type for the selected transmission.