Signal Studio software products do not provide direct connectivity for all licensed platforms. In these cases, waveforms must be created in simulated hardware mode, exported to a waveform file, and then loaded into the instrument's controlling PC via a USB storage device. This procedure describes how to create and transfer waveform files using this method and applies to the following instruments.
Keysight SystemVue ESL Design Software
Keysight M9381A PXIe Vector Signal Generator
Keysight M9252A DigRF Host Adapter
This procedure uses Keysight Signal Studio for LTE-LTE-Advanced FDD as an example, but the steps are valid for all Signal Studio software applications.
Open the software. The welcome dialog window appears.
If the welcome dialog window does not appear when the software is launched, click > and make sure is checked. Then close and re-open the software.
Select and highlight your instrument. Click .
Because simulation mode offers all possible capability options, the caution shown below may appear. Whether the caution appears or not, however, you must set any unpurchased licenses to , otherwise the generated waveform cannot be played back in the instrument. If your software's interface does not provide access to a node where this is performed, proceed to step 6.
In the software's tree view, click . Notice that in simulated hardware mode, all software licensing options are set to On.
In the State column, click the cell to turn off any options you did not purchase. This is necessary to create a valid waveform for playback on your instrument. This example assumes the advanced option was not purchased for your instrument.
|
Action |
|
|
Result |
|
Configure the Signal Studio waveform using the various parameter selections and settings available under the Waveform Setup node in the tree view. Waveform parameters vary among Signal Studio products, so refer to this help system for more information.
Click the button.
Under the File menu, select .
Name the waveform file and save it to your PC.
Copy the waveform file to a portable USB storage device.
This would be a good time to also save a backup copy of the waveform file.
Insert the USB storage device into a USB port on the controlling PC and copy the waveform file to the proper directory, as described in the instrument's documentation.