Select a DL-SCH channel in the Channel
Setup node, then click the
button in the Transmission
Configuration cell to open the DL-SCH Tx sequence window.
The DL-SCH TX window displays the transmission sequence defined in the Channel Setup node for the selected DL-SCH channel.
The settings configured in the Channel Setup node and the DL-SCH Tx sequence window are displayed in the Tx Map.
Use the button to navigate to and import a saved transmission sequence.
Use the button to save the current transmission sequence to a file.
Click the
button to access a
drop-down list
that enables you to set parameters for all transmissions to the same value.
See Parameter Descriptions below.
|
|
Choice: On | Off
Default: On
Double-click to turn on or off the transmission state for the current subframe.
Choice: On | Off
Default: Off
Double-click to turn on or off the retransmission state for Codeword 0.
Choice: On | Off
Default: Off
Double-click to turn on or off the retransmission state for Codeword 1.
Range: 0 to 31
Default: 0
Enter a value for the MCS Index for Codeword 0.
Range: 0 to 31
Default: 0
Enter a value for the MCS Index for Codeword 1.
Choice: QPSK | 16QAM | 64QAM
Default: QPSK
Use the drop-down menu to select the modulation type for Codeword 0.
Choice: QPSK | 16QAM | 64QAM
Default: QPSK
Use the drop-down menu to select the modulation type for Codeword 1.
Range: 0 to 26
Default: 0
Enter a value for the TBS Index for Codeword 0.
Range: 0 to 26
Default: 0
Enter a value for the TBS Index for Codeword 1.
Range: 1 to 86400
Default: 680
Enter a value for the transport Block Size for Codeword 0.
Range: 1 to 86400
Default: 680
Enter a value for the transport Block Size for Codeword 1.
Range: 0 to 3
Default: 0
Enter a value for the redundancy version (RV) index for Codeword 0.
Range: 0 to 3
Default: 0
Enter a value for the redundancy version (RV) index for Codeword 1.
Range: 0 to RBmax – 1
Default: 0
Enter the number of resource blocks by which to offset the DL-SCH sequence.
Range: 1 to RBmax
Default: 25
Enter the number of resource blocks in the frequency domain for the DL-SCH sequence.