To set up a fixed reference
channel (FRC), for an Advanced LTE TDD Uplink carrier, click the Wizard
button
in the Uplink Setup
node for the LTE
standards to open the FRC Wizard.
Double-click or use the drop-down menu to set the system bandwidth and number of resource blocks for the fixed reference channel.
Double-click or use the
drop-down menu to set the
FRC Type.
The software sets the parameters displayed in the lower section of the
window to predetermined values for the FRC Type and Reference Channel
"A" value (An-n) selected.
Double-click or use the
drop-down menu to set the Type A value (An-n) for the selected FRC Type. The software
sets the parameters displayed in the lower section of the window to predetermined
values for the FRC Type and
Reference
Channel
selected.
Range: 0 to the number of resource blocks determined by the System Bandwidth selection.
Default: 0
Set the resource block offset for the FRC.
Choice: Off | On
Default: Off
Double-click or use the drop-down menu to turn the sounding reference signal on or off.
Displays the allocated resource blocks for the selected FRC Type and Reference Channel 'A' value.
Displays the DFT-OFDM symbols per subframe.
Displays the modulation type for the selected FRC Type.
Displays the code rate for the selected FRC Type.
Displays the payload size for the selected FRC Type and Reference Channel 'A' value.
Displays the code block CRC size, in bits, for the selected FRC Type and Reference Channel 'A' value.
Displays the code block CRC size, in bits, for the selected FRC Type and Reference Channel 'A' value.
Displays the number of code blocks for the selected FRC Type and Reference Channel 'A' value.
Displays the coded block size for the selected FRC Type and Reference Channel 'A' value.
Displays the number of bits per subframe for the selected FRC Type and Reference Channel 'A' value.
Displays the number of symbols per subframe for the selected FRC Type and Reference Channel 'A' value.
Displays the maximum throughput, in kbps, for the selected FRC Type and Reference Channel 'A' value.