Real Time

Physical Signals

Physical signals are used by the physical layer, but do not carry information originating from higher layers.

Uplink Physical Signals

The two uplink physical signals are demodulation reference signals and sounding reference signals.

The same set of base sequences is used for the demodulation and sounding reference signals.

Downlink Physical Signals

There are two types of downlink physical signals: reference signals and synchronization signals.

Reference Signals

Downlink reference signals can be classified into three types:

One reference signal per antenna port is transmitted.

Synchronization Signals

Primary and secondary synchronization signals are transmitted in the downlink to enable the UE to acquire time and frequency synchronization with a cell.  

For more information about physical signals refer to the 3GPP LTE Technical Specifications documents at http://www.3gpp.org.