Select the DCI channel in the Channel
Setup node, then click the
button in the DCI
#10 for Random Access Procedure cell to open the RACH PDCCH Tx Setting
window.
The RACH PDCCH Tx Setting window displays the parameters setting of PDCCH transmitted in each subframe for the random access procedure.
Use the tab to navigate to and import a saved transmission sequence.
Use the tab to save the current transmission sequence to a file.
Click the
button to access a
drop-down list
that enables you to set parameters for all transmissions to the same value.
Click the links in the tables below for parameter descriptions.
|
2. PDCCH Settings |
|
|---|---|
|
|
|
|
|
|
|
|
|
Other Parameter Descriptions |
|---|
Double-click or use the drop-down menu to control the operating state of DCI channel.
The DCI for a Random Access Procedure uses DCI format 1A.
Display the Data Source of the DCI channel. The data for DCI is auto generated using the PRACH parameter setting in each subframe.
Display the payload size in bits. Refer to the 3GPP TS 36.212 5.3.3.1 DCI formats for more information.
Range: 1 to 65535
Default: 1
Enter a value for the Radio Network Temporary Identifier (RNTI).
Choice: UE Port 0 | UE Port 1
Default: UE Port 0
Double-click or use the drop-down menu to set the UE Tx Antenna for the DCI channel.
Choice: Common | UE Specific
Default: Common
Double-click or use the drop-down menu to set the search space of the PDCCH channels.
See more details about this parameter in the PDCCH Assignment Procedure in 3GPP TS 36.213 9.1.1.
Choice: Off | On
Default: On
Click to turn the DCI state on or off in the selected subframe.
Choice:0 to 63
Default: 0
Set Preamble Index in the selected subframe.
Choice: 0 to 15
Default: 15
Set PRACH Mask Index in the selected subframe.
Choice: 1 | 2 | 4 | 8
Default: 1
Select the Aggregation level for the DCI searching space in the selected subframe.
See more details about this parameter in the PDCCH Assignment Procedure in 3GPP TS 36.213 9.1.1.
Choice: 0
Default: 0 to maximum
Set the candidate within the searching space in the selected subframe.
See more details about this parameter in the PDCCH Assignment Procedure in 3GPP TS 36.213 9.1.1.
Display the CCE offset of the DCI in the selected subframe.
See more details about this parameter in the PDCCH Assignment Procedure in 3GPP TS 36.213 9.1.1.