Real Time

UCI Tx sequence Window (Advanced LTE-A TDD Uplink)

The UCI Tx sequence window displays the currently configured UCI transmission sequence. For the same UE, the UCI channel cannot be transmitted in subframes occupied by UL-SCH processes.

Select a UCI channel in the Channel Setup node, then click the button in the Transmission Configuration cell to open the UCI Tx sequence window.You can set parameters for each UCI transmission from within the UCI Tx sequence window.   

Grid Parameters

State

Format

RNTI

Modulation

Data/Control Type

Data

Data Size

HARQ-ACK

nPUCCH(1,0)

nPUCCH(3,0)

RB Location

DMRS Power

Parameter Descriptions

State

Click the cell to toggle the state of the UCI Tx sequence on or off.

Format

Choice: 1 | 1a | 1b | 2 | 2a | 2b | 3

Default: 1

Set the UCI format.

Enter a format number for the Tx sequence.

The Modulation type is set by the software based on the selected Format. See Modulation.

The choices available for the HARQ-ACK parameter are based on the selected Format. See HARQ-ACK.

See 3GPP TS 36.211, 36.212 and 36.213.

RNTI

Range: 0 to 65535

Default: 0

Enter a value for the Radio Network Temporary Identifier (RNTI). RNTI only applies to format 2/2a/2b. See 3GPP TS 36.211, 36.212 and 36.213 for more information.

Modulation

The modulation type for the UCI Tx sequence is set according to the active Format as follows:

Data/Control Type

The software sets the Data Type according to the active Format, as follows:

* Where: the UCI format is set to Format 1b and the UE is configured with a single serving cell, up to a HARQ-ACK (4-bit) channel selection can be set.

See 3GPP TS 36.211, 36.212 and 36.213 for more information.

Data

For Formats 2, 2a, or 2b, double-click in this cell to open a dialog box from which you can select PN9, PN15, or User Defined Bits as the data for the UCI Tx sequence.

Data Size

Range:

1 to 13-bits (Formats 2, 2a, 2b with Normal Cyclic Prefix or Format 2 with Extended Cyclic Prefix and CQI Data Type)

1 to 12-bits (Format 2 with Extended Cyclic Prefix and CQI + HARQ-ACK (1-bit) Data Type)

1 to 11-bits (Format 2 with Extended Cyclic Prefix and CQI + HARQ-ACK (2-bits) Data Type)

Enter a value for Data Size for Formats 2, 2a,or 2b.

HARQ-ACK

Choice:

ACK | NACK (Format 1a/2a)

ACK-ACK | ACK-NACK | NACK-ACK | NACK-NACK (Format 1b/2b)

ALL ACK | ALL NACK | User Defined Bits (Format 3)

Default:

ACK (Format 1a/2a)

ACK-ACK (Format 1b/2b)

ALL ACK (Format 3)

Specifies the HARQ-ACK information corresponding to PUCCH Format.

Double-click the HARQ-ACK cell for the sequence you want to configure to open the HARQ-ACK Info Selection dialog box. Select the radio button in the dialog box for the desired HARQ-ACK. The choices available for HARQ-ACK are determined by the active Format.

Refer  to 3GPP TS 36.211, 36.212 and 36.213.

nPUCCH(1,0)

Range: 0 to minimum (2047 or Calculated Maximum Value).

Depends on the related PUCCH values.

Default: 0

Enter a value for the PUCCH n(1) number.

Specifies the resource index for PUCCH formats 1/1a/1b.

Calculated maximum value means the resource is at the center of the system bandwidth.

Refer  to 3GPP TS 36.211, 36.212 and 36.213.

nPUCCH(3,0)

Range: 0 to (Number of resource blocks in the system bandwidth) * 5 – 1

Default: 0

Enter a value for the nPUCCH(3) number.

Specifies the resource index for PUCCH format 3.

Refer  to 3GPP TS 36.211, 36.212 and 36.213.

RB Location

Displays the numbers of the resource blocks occupied by the PUCCH, separated by a comma. If any of the following are changed: PUCCH Format, N_RB(2), N_CS(1), n(1), n(2), Delta Shift or Delta Offset, the resource block numbers are updated accordingly.

DMRS Power

Range: –60 to 0 dB

Default: 0 dB

Enter a power level in dB for the demodulation reference signal for the UCI Tx sequence.