Select the DCI channel in the Channel
Setup node, then click the
button in the DCI
#11 for Uplink Power Control cell to open the Uplink Power Control
PDCCH Tx Setting window.
The Uplink Power Control PDCCH Tx Setting window displays the parameters setting of PDCCH transmitted in each subframe for the selected Uplink Power Control PDCCH channel in the Channel Setup.
Use the Import tab to navigate to and import a saved transmission sequence.
Use the Export tab to save the current transmission sequence to a file.
Click the
button to access a
drop-down list
that enables you to set parameters for all transmissions to the same value.
Click the links in the table below for parameter descriptions.
|
1. DCI Settings |
2. PDCCH Settings |
|---|---|
|
|
|
|
|
|
|
|
|
Other Parameter Descriptions |
|---|
Double-click or use the drop-down menu to control the operating state of DCI channel.
Choice: Format 3 | Format 3A
Default: Format 3
Double-click or use the drop-down menu to set the format of the DCI.
DCI format 3 is used for the transmission of the TPC commands for PUCCH and PUSCH with 2-bits power adjustments.
DCI format 3A is used for the transmission of the TPC commands for PUCCH and PUSCH with 1 bit power adjustments.
Display the Data Source of the DCI channel. The data for DCI is auto generated using the TPC bits content in each subframe.
Display the payload size in bits. Refer to the 3GPP TS 36.212 5.3.3.1 DCI formats for more information.
Range: 1 to 65535
Default: 1
Enter a value for the Radio Network Temporary Identifier (RNTI).
Choice: UE Port 0 | UE Port 1
Default: UE Port 0
Double-click or use the drop-down menu to set the UE Tx Antenna for the DCI channel.
Choice: Common | UE Specific
Default: Common
Double-click or use the drop-down menu to set the search space of the PDCCH channels.
See more details about this parameter in the PDCCH Assignment Procedure or refer to 3GPP TS 36.213.
Choice: Off | On
Default: On
Click to turn the DCI state on or off in the selected subframe.
Choice: System bandwidth dependent
Default: ”00000000000000000000000000”
Set TPC command bits of the transmission in the selected subframe.
DCI format 3 is used for the transmission of the TPC commands for PUCCH and PUSCH with 2-bits power adjustments.
DCI format 3A is used for the transmission of the TPC commands for PUCCH and PUSCH with 1 bit power adjustments.
The following information is transmitted by the means of the uplink power control DCI formats:
TPC command number 1, TPC command number 2, ... , TPC command number n
Choice: 1 | 2 | 4 | 8
Default: 1
Select the Aggregation level for the DCI searching space in the selected subframe.
See more details about this parameter in the PDCCH Assignment Procedure in 3GPP TS 36.213 9.1.1.
Choice: 0
Default: 0 to maximum
Set the candidate within the searching space in the selected subframe.
See more details about this parameter in the PDCCH Assignment Procedure in 3GPP TS 36.213 9.1.1.
Display the CCE offset of the DCI in the selected subframe.
See more details about this parameter in the PDCCH Assignment Procedure in 3GPP TS 36.213 9.1.1.