Real Time

Uplink Resource Block

Figure 1 illustrates an uplink resource block made up of resource elements. Each resource element corresponds to an SC-FDMA symbol. An index pair (k,l) defines a resource element, where k represents the resource element position in the frequency domain and l represents the resource element position in the time domain.

An uplink resource block is defined as consecutive SC-FDMA symbols in the time domain, and consecutive subcarriers in the frequency domain. This corresponds to one slot in the time domain and 180 kHz (12 subcarriers x 15 kHz per subcarrier) in the frequency domain. The number of SC-FDMA symbols in a slot () depends on the cyclic prefix as shown in the table below.

Refer to the 3GPPTS 36.211 document for more information about resource blocks.

CP

(frame structure type 1)

(frame structure type 2)

Normal cyclic prefix

12

7

9

Extended cyclic prefix

12

6

8

Figure 1. Uplink Resource Block