Real Time

PUSCH Settings

When using multiple instruments as shown in the tree view, inaccurate test data may occur if a combination of the GUI and SCPI is used to set or modify the instrument and test parameters. The software will not reflect changes made outside of the GUI even with the use of the Update from Instrument button. For all tests, use only one method to configure the settings, GUI or SCPI.

When configuring multiple instruments with SCPI instead of using the GUI, the commands must be executed for each instrument.

When using multiple instruments as shown in the tree view, after clicking the State On button, all settings for this window gray out and cannot be changed. To change the settings, first click the State Off button.

1. PUSCH Settings

2. Transmission Settings

3. Demodulation Reference Signal Settings

State

Occupied Resource Block Size

DMRS Power

Power

Occupied Resource Block Offset

Delta SS

 

 

nDMRS(1)

 

 

nDMRS(2)

 

 

Cyclic Shift Field in Uplink-Related DCI Format

 

 

Activate-DMRS-with OCC

 

 

OCC [w(0) w(1)]

Buttons

This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. When using multiple instruments as shown in the tree view, this button is not displayed.

This button displays in place of the Settings Current button. It indicates that the instrument settings are not currrent and need to be updated with the new software settings. Click this button to update the insturment's settings. This button shows in all windows regardless of where the change was made. When using multiple instruments as shown in the tree view, this button is not displayed.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:APPLy

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:APPLy?

1. PUSCH Settings

State

Choice: Off | On

Default: On

Double-click or use the drop-down menu to select the state for the PUSCH.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:STATe 1|0|ON|OFF

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:STATe?

Power

Range: -60 to 20 dB

Default: 0 dB

Enter a power level in dB for the selected channel relative to the carrier power.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:POWer <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:POWer?

2. Transmission Settings

Occupied Resource Block Size

Range: 1 to 6 (1.4MHz BW), 1 to 15 (3MHz BW), 1 to 25 (5MHz BW), 1 to 50 (10MHz BW), 1 to 75 (15MHz BW), 1 to 100 (20MHz BW)

Default: 6 (1.4MHz BW), 15 (3MHz BW), 25 (5MHz BW), 50 (10MHz BW), 75 (15MHz BW), 100 (20MHz BW)

Enter an integer between 1 and the maximum  number of resource blocks. The maximum value depends on the current transmission bandwidth.

For more information, refer to TS 36.101.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ORBLock:SIZE <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ORBLock:SIZE?

Occupied Resource Block Offset

Range: 0 to 5 (1.4MHz BW), 0 to 14 (3MHz BW), 0 to 24 (5MHz BW), 0 to 49 (10MHz BW), 0 to 74 (15MHz BW), 0 to 99 (20MHz BW)

Default: 0

Enter the number of resource blocks to offset the transmission of this UE.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ORBLock:OFFSet <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ORBLock:OFFSet?

3. Demodulation Reference Signal Settings

DMRS Power

Range: -60 to 20 dB

Default: 0 dB

Enter a power level in dB for the power of Demodulation Reference for PUSCH to the carrier power.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DMRSignal:POWer <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DMRSignal:POWer?

Delta SS

Range: 0 to 29

Default: 0

This value is used to calculate the sequence-shift pattern. For more information, refer 3GPP TS36.211 for more details.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DELTa:SS <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DELTa:SS?

nDMRS(1)

Choice: 0 | 2 | 3 | 4 | 6 | 8 | 9 | 10

Default: 0

Enter a value to calculate a PUSCH DMRS data pattern. For more information, refer 3GPP TS36.211 for more details.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DMRSignal:N[1] <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DMRSignal:N[1]?

nDMRS(2)

Choice: 0 | 2 | 3 | 4 | 6 | 8 | 9 | 10

Default: 0

Coupling: A change to the Cyclic Shift Field in Uplink-Related DCI Format value or the Antenna Port Number may change this value.

Enter a value to calculate a PUSCH DMRS data pattern. Refer 3GPP TS 36.211 for more details.

When using multiple instruments as shown in the tree view, this setting is a display only parameter where its value is calculated by the software using the Cyclic Shift Field in Uplink-related DCI and Antenna Port settings.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DMRSignal:N2 <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:DMRSignal:N2?

Cyclic Shift Field in Uplink-Related DCI Format

Choices: 0 [000] | 1 [001\ | 2 [010] | 3 [011] | 4 [100] | 5 [101] | 6 [110] | 7 [111]

Default: 0 [000]

Coupling: A change to the nDMRS(2) value may change this value.

Double-click or use the drop-down menu to select a value. This value determines the OCC [w(0) w(1] setting. For more information, refer to TS 36.211.

When using multiple instruments as shown in the tree view, this setting is the same for all instruments.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh[1]:DMRSignal:DCI:CSField <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh[1]:DMRSignal:DCI:CSField?

Activate-DMRS-with OCC

Choices: Off | On

Default: Off

Set the state of the higher-layer parameter Activate-DMRS-with OCC. When set to On, orthogonal cover code (OCC) is applied to the DMRS.

[:SOURce]:RADio:LTE:TDD[:BBG]:LINk:PUSCh[1]:DMRSignal:OCC:STATe 0|1|OFF|ON

[:SOURce]:RADio:LTE:TDD[:BBG]:LINk:PUSCh[1]:DMRSignal:OCC:STATe?

OCC [w(0) w(1)]

Displays the [w(0) w(1)] list of OCC for the DMRS code generation.When Activate-DMRS-with OCC is set to Off, this displays [1 1]. For more information, refer to TS 36.211.