Real Time

UL-SCH—General Settings

When using multiple instruments as shown in the tree view, inaccurate test data may occur if a combination of the GUI and SCPI is used to set or modify the instrument and test parameters. The software will not reflect changes made outside of the GUI even with the use of the Update from Instrument button. For all tests, use only one method to configure the settings, GUI or SCPI.

When configuring multiple instruments with SCPI instead of using the GUI, the commands must be executed for each instrument.

When using multiple instruments as shown in the tree view, after clicking the State On button, all settings for this window gray out and cannot be changed. To change the settings, first click the State Off button.

1. UL-SCH Settings

2. HARQ-ARQ Settings

3. Hybrid-ARQ ACK/NACK Data Settings

Payload Data

Maximum Number of Retransmissions

Data Source

Modulation Type

Initial ACK Process Length

Data

Payload Configuration Type

RV Index Sequence

Input Delay (AUX Multiplexed Mode)

MCS Index

 

Input Delay (AUX Dedicated Mode)

TBS Index

 

Data Default Value (AUX Dedicated Mode)

Payload Size (bits)

 

 

Buttons

This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. When using multiple instruments as shown in the tree view, this button is not displayed.

This button displays in place of the Settings Current button. It indicates that the instrument settings are not currrent and need to be updated with the new software settings. Click this button to update the insturment's settings. This button shows in all windows regardless of where the change was made. When using multiple instruments as shown in the tree view, this button is not displayed.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:APPLy

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:APPLy?

1. UL-SCH Settings

Payload Data

Choice: PN9 | PN15 | Custom Pattern | User Defined

Default: PN9

Click the parameter and then use the button to launch the data dialog box.

PN9

Uses PN9 sequence as data bits

PN15

Uses PN15 sequence as data bits

Custom Pattern

Uses the user defined pattern specified in string and '0' or '1' is expected in the string pattern

User Data

Uses a user-defined sequence in a file as data bits

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:TYPE PN9|PN15|PATTern|FILE

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:TYPE?

If PATTern is the data type selection, use the following command to set the pattern. To set the pattern, use a series of 0, 1, or a combination of the two, 011100110, up to a maximum of 128,000 bits.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:PATTern <pattern>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:PATTern?

If FILE is the data type selection, use the following commands to load a previously saved file, and to set what length of the file to use.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:NAME <"filename">

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:NAME?

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:LENGth <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:DATA:FILE:LENGth?

Modulation Type

Choice: QPSK | 16QAM | 64QAM

Default: QPSK

When Payload Configuration Type in UL-SCH channel is set to Manual, double-click or use the drop-down menu to select the modulation type for the PUSCH. When the Payload Configuration Type in the UL-SCH channel is set to MCS Index, this value is calculated by the MCS Index. Refer 3GPP TS36.211, Table 8.6.1-1 for more details.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:MODulation QPSK|QAM16|QAM64

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:MODulation?

Payload Configuration Type

Choice: MCS Index | Manual

Default: MCS Index

Double-click or use the drop-down menu to select the UL-SCH Payload Configuration Type.

MCS Index

Selects a payload size determined by the Table 7.1.7.2.1-1 ( 3GPP TS36.213) which specifies the permissible combinations of transport block size, resource allocation and modulation scheme that are available for transmission.

Manual

Allows you to enter any payload size within the minimum (16) and maximum limits (75376) of Table 7.1.7.2.1-1 (3GPP TS36.213). 

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:CONFig MINDex|MANual

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:CONFig?

MCS Index

Range: 0 to 28

Default: 5

Enter a value of MCS Index. This parameter is used when the Payload Configuration Type is MCS is set to MCS Index.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:MINDex <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:MINDex?

TBS Index

Displays the value of TBS index. The value is calculated by the MCS Index, Refer to 3GPP TS36.211, Table 8.6.1-1 for more details. This parameter is used when the UL-SCH Payload Configuration Type is set to MCS Index.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:TINDex?

Payload Size (bits)

Range: 16 to 75376

Default: 2216

Coupling: The Configuration Type selection determines whether this setting is display only or active.

Displays the payload size when the UL-SCH Payload Configuration Type is set to MCS Index. With MCS Index, the payload size is determined by the size of occupied resource blocks and the MCS Index. Refer to 3GPP TS36.213 for more detailed information.

Enter a value to set the payload size when the UL-SCH Payload Configuration Type is set to Manual.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:SIZE <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:PAYLoad:SIZE?

2. Hybrid-ARQ Settings

Maximum Number of Retransmissions

Range: 0 to 27

Default: 3

Enter the maximum number of times for the uplink shared channel to be retransmitted.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:MNRetrans <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:MNRetrans?

Initial ACK Process Length

Range: 0-65535

Default: 8

Enter the HARQ ACK initial response length. The software uses this setting when the Data Source selection is External.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:PROCess:LENgth:IACK <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:PROCess:LENgth:IACK?

RV Index Sequence

Default: 0, 2, 3, 1

Entry format: Array of RV Index (Integer 0-3)

Array length: 1 to 28

Enter the RV (redundancy version) Index sequence pattern for verifying HARQ responses. The RV Index data can be entered as a sequence with values of 0, 1, 2, 3 separated by commas. When the specified length of RV index sequence pattern is shorter than the maximum number of retransmission, the pattern is repeated until reaching the maximum length.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:RVINdex:PATTern:DATA <val>

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:RVINdex:PATTern:DATA?

3. Hybrid-ARQ ACK/NACK Data Settings

Data Source

Choice: Internal | External

Default: Internal

Double-click or use the drop-down menu to select HARQ ACK/NACK control signal source.

Internal

Uses an internal user-defined signal.

External

Uses an external signal from AUX ports.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:SOURce INTernal|EXTernal

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:SOURce?

Data

Choice: All ACK| All NACK| Custom Pattern| User Data

Default: All ACK

Coupling: Active when Data Source is set to Internal.

Click the parameter and then use the button to launch the data dialog box.

All ACK

All ACK sequence

All NACK

All NACK sequence

Custom Pattern

Uses the user defined pattern specified in string and 'A' or 'N' is expected in the string pattern

User Data

Select a user-defined sequence from an existing file on the local drive

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:TYPE AACK|ANACk|FILE|PATTern

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:TYPE?

If FILE is the selection, use the following command to load an existing file for the ACK/NACK data.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:FILE:NAME <"filename">

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:FILE:NAME?

If PATTern is the selection, use the following command to create the custom pattern with a maximum of 8,192 characters. The pattern is a string that uses "A" (ACK), "N" (NACK), or a combination "ANNANAA".

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:PATTern <"pattern">

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:INTernal:DATA:PATTern?

Input Delay (AUX Multiplexed Mode)

Displays the fixed delay time (0)of the input port for control of the HARQ ACK/NACK. The delay time is displayed when the HARQ ACK/NACK Data Source is set to External and the AUX Operating Mode is set to Multiplexed.

Input Delay (AUX Dedicated Mode)

Displays the fixed delay (0) of the HARQ ACK response in the serial data transmission. The unit of delay is in subframe. The delay is displayed when the HARQ ACK/NACK Data Source is set to External and the AUX Operating Mode is set to Dedicated.

Data Default Value (AUX Dedicated Mode)

Choice: Choice: NACK | ACK

Default: NACK

Coupling: Grayed out unless Operating Mode is set to Dedicated and Data Source is set to External.

Double-click or use the drop-down menu to select the default value for the HARQ ACK/NACK response when the feedback signal is not received.

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:EXTernal:DATA:SERial:DEFault ACK|NACK

[:SOURce]:RADio:LTE:TDD[:BBG]:ULINk:PUSCh:ULSCh:HARQ:EXTernal:DATA:SERial:DEFault?