Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to topic

Carrier

1. General Settings

Enabled

Select/ deselect the Enable check box to enable/ disable the channel or signal in a radio frame.

Power

Range: -40 - 40dB

Default: 0dB

Set the power of the carrier relative to others.

System Sample Frequency

Display the system sampling rate in Hz.

Initial Phase

Range: 0 - 360

Default: 0

Enter the initial phase of the carrier signal in degree.

Frequency Offset

Default: 0

Enter the frequency offset to the carrier signal in Hz. The max absolute offset is limited by System Sample Frequency * Oversampling Ratio / 2.56 - Actual Bandwidth / 2. (For VZW, actual bandwidth of each carrier is 99MHz.)

Timing Offset

Range: 0 - Frame length

Default: 0

Set the timing offset of the carrier relative to others.

2. Cell Settings

Cell ID

Range: 0 - 503

Default: 0

Set the cell ID for the carrier. Cell ID is calculated by Cell ID = 3 * N_ID(1) + N_ID(2).

Subcarrier Spacing

The Subcarrier spacing field displays the subcarrier spacing.

Number of Symbols for Resource Block

The Number of Symbols for Resource Block field displays the number of OFDM symbols in one resource block.

Number of Subcarriers for Resource Block

The Number of Subcarriers for Resource Block field displays the number of subcarriers in one resource block.

Total Number of Resource Blocks

The Total Number of Resource Blocks field displays the total number of resource blocks for one carrier.

Total Number of Occupied Subcarriers

The Total Number of Occupied Subcarriers field displays the total number of occupied subcarriers for one carrier.

3. Spectrum Control

Filter

Choices: None | Gaussian | Root Nyquist | Nyquist | Rectangle | User Defined

Default: None

Select the filter type to be applied to the waveform. The OFDM Filter Editor dialog appears.

You can view the impulse response and frequency response in the filter editor.

Window Beta

Range: 0 - 0.5

Default: 0.01

Set the windowing length used to smooth OFDM symbol transitions. Specify this value as a fraction of FFT Length, not the percentage.

Windowing Method

Choices: Centered at Symbol Boundary | Starting at Symbol Boundary

Default: Centered at Symbol Boundary

Select the windowing method applied to the OFDM symbol transitions. The raised cosine window can be centered at the OFDM symbol boundary, or starting from the OFDM symbol boundary.

Graph View

The graph view displays several different representations of the generated waveform. For more information, see Graph View.

89600 Setup File Setting

OFDM Filter Editor