xPRACH Configuration
When customers add an xPRACH subframe configuration, all the other existing subframe configurations are set to off and can’t be turned on until the xPRACH configuration is off, we assume that xPRACH can’t be transmitted with other channels simultaneously.
1. xPRACH
Enable
Select/ deselect the Enable check box to enable/ disable the channel or signal in a radio frame.
Power Boosting
Range: -40 - 40
Default: 0
Set the additional power boosting for the channel.
Antenna Port
Set the antenna port on which the symbols will be generated into the waveform.
Configuration Index
Range: 0 - 3
Default: 0
Set the PRACH configuration index.
Preamble Format
Range: 0 - 1
Default: 0
Set the PRACH preamble format.
RACH Cyclic shift v
Range: 0 - 2 for format 0; 0 for format 1.
Default: 0
Set the RACH cyclic shift v.
RACH Zadoff-Chu Root u
Range: 0 - 1000
Default: 0
Set the RACH Zadoff-Chu Root u.
RACH subband index n_RACH
Range: 0 - 7
Default: 0
Set the RACH subband index n_RACH.
RACH Parameter f'
Range: 0 - 1
Default: 0
Set the RACH parameter f'.
Symbol Index l
Choice: 0,1 | 2,3 | 4,5 | 6,7 | 8,9 for format 0; 0,1 | 2,3| 4,5 | 6,7 for format 1.
Default: 0,1
Select the symbol index for RACH transmission.
2. Scheduling Request Collection
SR Transmit Control
Choice: Enabled | Disabled | Only.
Default: Enabled
Control the Scheduling Request in xPRACH.
SR Zadoff-Chu Root u
Range: 0 - 1000
Default: 0
Set the scheduling request Zadoff-Chu Root u.
SR Cyclic shift v
Range: 0 - 11.
Default: 0
Set the scheduling request cyclic shift v.
SR Parameter f'
Range: -1, 1
Default: 1
Set the scheduling request parameter f'.
SR subband index N_SR
Range: 0 - 7
Default: 0
Set the scheduling request subband index N_SR.