Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Waveform Setup

Click Waveform Setup in the tree view to display the waveform pane shown below. The waveform setup pane is divided into three sections: Carrier Configuration Summary Table (top), Waveform Setup Property Grid (middle), and Graph View (bottom).

Add Carrier

Choices: NR Downlink | NR Uplink | NR PRACHContinuous Wave

Click the ClosedAdd Carrier button to add a new 5G NR carrier to the list. New carrier will be assigned with a different Cell ID based on current carrier count.

Maximum carrier number is 16.

Remove Carrier

Click the Remove Carrier button to delete the selected 5G NR carrier from the list.

Copy Carrier

Click the Copy Carrier button to copy the selected 5G NR carrier and append it to the list.

Auto Frequency Offset

This Closeddrop-down menu allows you to automatically set the frequency offset for each carrier, based on section 5.4.1 of 38.104, to get the expected channel spacing.

Save to 89600 Setup File

This feature saves the Carrier configuration as a 89600B VSA setup file, simplifying VSA configuration so you can quickly demodulate the signal. For information about setup file settings, refer to 89600 Setup File Setting.

Carrier Configuration Summary Table

This table enables you to view the key properties for each carrier in the waveform. You can also add or delete carriers using the buttons above the table (see descriptions above). Double-click a carrier row to access the properties for that carrier.

1. Basic

Playback License Mode

Choices: PC License | Instrument License

Default: PC License.

Select the playback license mode. If no PC license is available, only Instrument License can be used.

Licensing of Signal Studio Pro Software

 

N76xxAPPC

N76xxEMBC

License File Presence

PC

(running Signal Studio Pro software)

Signal Generator

Playback License Mode

Two selections

(PC License | Instrument License)

One selection

(Instrument License)

Available Software

Functions

Live Connection to Signal Generator

ü

ü

VSA .SETX Export

ü

ü

Programming API

ü

ü

Waveform Export

ü

ü

License Mode Switching

You can switch waveform playback license mode to take advantage of an instrument license, even when a PC license is available with GUI parameter "Playback License Mode" under "Waveform Setup" node, "Basic" group.

3GPP Version

Default (fixed): V16.2.0 (2020-06)

This read-only field display the supported version of 3GPP specifications:

TS 38.211 Physical Channels and Modulation

TS 38.212 Multiplexing and Channel Coding

TS 38.213 Physical Layer Procedures for Control

TS 38.214 Physical Layer Procedures for Data

Capability

Choice: Waveform Playback | Real-time Uplink

Default: Waveform Playback

Select the capability of 5G signal simulation.

Waveform Comment

Enter the comment for the waveform, up to 32 characters.

User Defined Sample Rate

Choice: On | Off

Default: Off

Enable or disable the User Defined Sample Rate. If enabled, the Sample Rate can be edited to input the user defined sample rate.

Sample Rate

Range: 20 MHz to 12 GHz

Default: 122.88 MHz (61.44 MHz if numerology = 15 kHz)

This parameter is read-only. The sample rate is automatically calculated to meet the requirement of waveform settings and connected instrument.

If User Defined Sample Rate is disabled, the sample rate is automatically calculated to meet the requirement of waveform settings and connected instrument, otherwise this value can be editable to input user-defined sample rate.

Time Scale Factor

Range: 0.001 to 1000

Default: 1

Set the Time Scale Factor of the sample rate.

When Phase Compensation is set to Auto (Real-time) or Manual (Real-time) this parameter is read-only and set to 1.

Number of Radio Frames

Default: 1

If the carrier is a downlink carrier and SSB is enabled, change this parameter to match the SSB period, otherwise a warning is generated.

When the Number of Radio Frames is not 1, different configurations for different frames are supported. For SS/PBCH, the multi-frame configuration is determined by the SSB period. For other channels, edit the Allocated Slots field to set multi-frame configuration.

Subframe Offset

Range: 0 to 9

Default: 0

Set the subframe offset to generate partial radio frame when the Number of Radio Frames is 1.

Number of Subframes

Range: 1 to (10 - Subframe Offset)

Default: 10

Set the number of subframes to generate partial radio frame when the Number of Radio Frames is 1.

Slot Offset in Subframe

Set the slot offset in subframe to generate partial subframe when the number of subframe is 1. This parameter is only applicable for single downlink/uplink carrier and single numerology case.

The range is based on the numerology of the carrier.

Number of Slots in Subframe

Set the number of slots in subframe to generate partial subframe when the number of subframe is 1. This parameter is only applicable for single downlink/uplink carrier and single numerology case.

The range is based on the numerology of the carrier.

Total Sample Points

Sets or displays the number of sample points in the waveform. This value can be edit if there is no carrier in the waveform, otherwise it is read-only and will be automatically updated with waveform setting changes.

Waveform Length

Display the waveform length in seconds. This value is read-only and will be automatically updated with waveform setting change

Mirror Spectrum

Choices: On | Off

Default: Off

If enabled, I and Q data of waveform are swapped to make the mirror spectrum. PSG has I/Q Swap at 20G~28.5G band, so this should be enabled for testing signal from PSG at 28 GHz.

Phase Compensation

Choices: Auto | Auto (Real-time) | Manual | Manual (Real-time) | Off

Default: Auto

Set the phase compensation mode on the baseband signal before upconversion. Phase compensation is not applicable for PRACH carrier.

Auto (Real-time) and Manual (Real-time) Information

See also, Real-time Phase Compensation Using SCPI.

Radio Frequency

Range: 0 to 100 GHz

Default: 1 GHz

Set the Radio Frequency when doing the phase compensation on baseband signal, it is automatically coupled with the frequency of instrument when Phase Compensation is set to Auto, and can be edited when Phase Compensation is set to Manual, but not visible when Phase Compensation is Off.

Total Number of Antennas

Choices: 1 | 2 | 3 | 4

Default: 1

Sets the number of antennas for each generation. It is used for MIMO configuration. The "Antenna Port(s) Generated" parameter in the Channel Setup node for DL-SCH, ULSCH, CSI-RS, and SRS allows you to configure the mapping between antenna and logical antenna port.

2. Marker

Marker 1 Source

Choices: Waveform Start | Frame Start | RF Blanking Control | RF ALC Control

Default: Waveform Start

Select the source for marker 1.

Marker 2 Source

Choices: Waveform Start | Frame Start | RF Blanking Control | RF ALC Control

Default: Frame Start

Select the source for marker 2.

Marker 3 Source

Displays the source for marker 3. RF Blanking Control is always used as Marker 3 source.

Marker 4 Source

Displays the source for marker 4. RF ALC Control is always used as Marker 4 source.

3. Crest Factor Reduction

Crest Factor Reduction

Choices: On | Off

Default: Off

Enable or disable the crest factor reduction for the waveform. When enabled, peak cancellation algorithm is used to subtract a weighted version of the cancellation pulses from the original input signal. It strikes a balance between the out-of-band emission and in-band waveform quality when reducing the PAPR of the signal.

When Phase Compensation is set to Auto (Real-time) or Manual (Real-time) this parameter is read-only and set to Off.

Target PAPR

Range: 3 to 100 dB

Default: 8 dB

Set the PAPR value to achieve after crest factor reduction.

Max Iteration

Range: 1 to 100

Default: 10

Specify the maximum times of iteration. With the increase of iteration, the PAPR value should converge to a steady level.

Cancelling Percent

Range: 0 to 100%

Default: 100%

Specify the percentage of the cancellation pulses that can be removed.

Block Size

Range: 20 to Waveform Total Sample Points

Default: 1000

Block is the range so that a single cancellation pulse can be identified. If the waveform length is L, and the block size is B, then the number of blocks is N=floor(L/B)+1. Therefore, there will be N pulses at most to be removed.

Filter Mask

Bring up the filter mask Closededitor to define a filter response in frequency domain. In the table, the frequency points must be entered with an order of increasing frequency in unit of MHz, and its corresponding amplitude is in unit of dB. When generating this filter mask, the frequency points between the specified points are linearly interpolated. When carrier number or carrier frequency offset in the waveform is changed, this table is automatically updated. A need may arise to adjust the mask manually to fit the actual signal bandwidth.

4. AWGN Setup

Enabled

Choices: On | Off

Default: Off

Enable or disable additive white gaussian noise (AWGN) in the waveform.

Carrier to Noise Ratio

Range: -100 to 100 dB

Default: 0 dB

Set the carrier to noise ratio, where the carrier is the one with 0dB power.

Carrier Bandwidth

Range: 1 to Sample Rate

Set the waveform bandwidth, it is automatically updated when parameters related to frequency domain location changes, otherwise user can input self-defined value.

Flat Noise Bandwidth

Range: 1 to Sample Rate / 1.25

Set the noise bandwidth.

Flat Noise Power Offset

Display the flat noise power offset compare to the signal generator power.

Carrier Power Offset

Displays the carrier power offset compare to the signal generator power.

Graph View

The graph view displays several different representations of the generated waveform. For more information, see Graph View.