Real Time

Waveform Graph

Click Waveform Setup or Carrier in the Closedtree view. The graph view is located below the Waveform Setup property grid. Click the Waveform tab to display the waveform graph.

Click Generate Waveform or Generate and Download from the main tool bar to generate an I/Q waveform and plot four different waveform graphs (Power, I+Q, I/Q, and Spectrum) for the current waveform configuration. Changes to the waveform configuration do not update the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform generation progress.

The Power plot is shown in the figure below.

Click the down arrow to open a Closeddrop-down menu from which you can select other waveform plots. Selections include Power (shown above), I+Q, I|Q, and Spectrum. Click the button to the left of the arrow to advance to the next plot type in the list without displaying the menu.

CCDF Graph