Real Time

Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Waveform Setup

Graph View

1. Mode

PHY Specification

Choices: 802.11ay EDMG | 802.11ad DMG

Default: 802.11ay EDMG

Select the format of PHY specification of the Millimeter Wave WLAN. For parameter descriptions, see the following:

802.11ay EDMG

802.11ad DMG

2. Basic

Waveform Name

Enter an alpha-numeric waveform file name of up to 22 characters. (If you enter a name with more than 23 characters, the software truncates the name to 22 characters when you click outside of the cell.) The name can include spaces and the following special characters: _ $ & # + - [ ].

Comment

Enter an alpha-numeric comment of up to 32 characters. The comment resides in the file header and can include spaces and special characters.

Number of Frames

Range: 1 to 300

Default: 1

Enter the number of frames included in the waveform.

Total Sample Points

Display the number of sample points in the waveform. This value is read-only and will be automatically updated with waveform setting change.

Waveform Length

Display the waveform length in seconds. This value is read-only and will be automatically updated with waveform setting change.

Mirror Spectrum

Choices: On | Off

Default: Off

Enable or disable the mirror spectrum (inverted IQ) for the waveform.

3. Marker

Marker 1 Source

Choices: Waveform Start | Frame Start | RF Blanking Control | RF ALC Control

Default: Waveform Start

Select the source for marker 1.

Marker 2 Source

Choices: Waveform Start | Frame Start | RF Blanking Control | RF ALC Control

Default: Frame Start

Select the source for marker 2.

Marker 3 Source

Default: RF Blanking Control

Displays the source for marker 3. RF Blanking Control is always used as Marker 3 source.

Marker 4 Source

Default: RF ALC Control

Displays the source for marker 4. RF ALC Control is always used as Marker 4 source.

Graph View

The graph view displays several different representations of the generated waveform. For more information, see Graph View.