Your Test Case Manager software license file (*.lic) is a text file that is attached to the email message you receive when you redeem your license. The license file is specific to the target Windows operating system (PC or Windows-based instrument) and Host ID.
Before installing the license file, save a backup copy in a safe place.
Save the license file to a convenient location on the host PC.
From the Start menu in Windows, launch Keysight License Manager.
After the Keysight License Manger opens, verify that the Host ID matches the host PC you are trying to license.
Within Keysight License Manager select > to open the Install License File(s) dialog box.
Use the Install License File(s) dialog box to navigate to the location where you placed the license file (*.lic) in Step 1.
Select the license file and click .
Wait for the license to appear in the Local Licenses list. This indicates that the license has been successfully installed on the PC.
Refer to the Keysight License Manager online help for more information about using the software.