Applicable Models: N522xB, N523xB, N524xB, E5080A/B (Read-Write) Sets and returns the status of the LXI LAN status indicator on the LAN Status dialog.  | 
		
	|
Parameters  | 
		
  | 
	
<bool>  | 
		Choose from: OFF or 0 - Changes the LXI Status indicator to ‘NORMAL’ and closes the dialog if it was opened by this command. ON or 1 - Changes the LXI Status indicator to ‘IDENTIFY’ and opens the dialog if it was not already open.  | 
	
Examples  | 
		LXI:IDEN 
		 1  | 
	
Query Syntax  | 
		LXI:IDENtify[:STATe]?  | 
	
Return Type  | 
		Boolean  | 
	
OFF  | 
	|