These commands control bandwidth, DUT information, avoid spurious function, and sweep.
|
SENSe:TDR BWIDth DLENgth | AUTO | DATA SPURious | AVOid | STATe? | INPut | DRATe | STATe? SWEep | AVERage | MODE | SINGLe
|
Click on a red keyword to view the command details.
See Also
|
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the IF bandwidth value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
<value> |
IF bandwidth value in Hz. |
|
Examples |
SENS:TDR:BWID:RES 100E3 |
|
Query Syntax |
SENSe<cnum>:TDR:BWIDth[:RESolution]? |
|
Return Type |
Double |
|
Default |
100 kHz |
|
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes auto DUT length setting. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
Examples |
SENS:TDR:DLEN:AUTO:IMM |
|
Default |
Not Applicable |
|
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the DUT length value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
<value> |
DUT length value in seconds. The range is 6.26n to 416n |
|
Examples |
SENS:TDR:DLEN:DATA 6.26E-9 |
|
Query Syntax |
SENSe<cnum>:TDR:DLENgth:DATA? |
|
Return Type |
Double |
|
Default |
6.26n |
|
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes avoid spurious. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
Examples |
SENS:TDR:SPUR:AVO:IMM |
|
Default |
Not Applicable |
|
Applicable Models: All with TDR Options (S9x011A/B) (Read-only) This command queries the avoid spurious state. This command is used only with Hot TDR mode.
|
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
Examples |
SENS:TDR:SPUR:AVO:STAT? |
|
Return Type |
Boolean 1 - ON 0 - OFF |
|
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the value of input bit rate for avoid spurious. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
<value> |
Value of input bit rate in bits per second (bps). The range is 1.21E6 to 60.8E9. |
|
Examples |
SENS:TDR:SPUR:INP:DRAT 1.5E9 |
|
Query Syntax |
SENSe<cnum>:TDR:SPURious:INPut:DRATe? |
|
Return Type |
Double |
|
Default |
1E9 |
|
Applicable Models: All with TDR Options (S9x011A/B) (Read-only) This command queries the Hot TDR mode status.
|
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
Examples |
SENS:TDR:SPUR:STAT? |
|
Return Type |
Boolean 1 - ON 0 - OFF |
|
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the TDR averaging trigger state on/off. When averaging trigger is on, one trigger makes one averaging measurement. For example, if the averaging factor is set at 16, one trigger makes a measurement 16 times. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
<bool> |
ON or 1 - Turns averaging trigger on. |
|
Examples |
SENS:TDR:SWE:AVER ON |
|
Query Syntax |
SENSe<cnum>:TDR:SWEep:AVERage? |
|
Return Type |
Boolean |
|
Default |
OFF |
|
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets trigger mode. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
<enum> |
Trigger mode. Choose from: HOLD - Trigger is on hold until the conditions are met, then the trigger event starts. SINGle - Trigger event is run once. RUN - Trigger event runs continuously. |
|
Examples |
SENS:TDR:SWE:MODE RUN |
|
Query Syntax |
SENSe<cnum>:TDR:SWEep:MODE? |
|
Return Type |
String |
|
Default |
RUN |
|
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes single trigger. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
|
Examples |
SENS:TDR:SWE:SING |
|
Default |
Not Applicable |