These commands control loss compensation, fixture compensation after an ECal, auto port extension, and reference impedance value.
SENSe:CORRection:TDR COLLection | DLComp | LOAD | OPEN | SAVE | THRU | ECAL | FCOMp EXTension | AUTO | STANdard
|
Click on a red keyword to view the command details.
See Also
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes load measurement, as a part of Loss Compensation sequence. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<int> |
Port number where load measurement is executed. The range is 1 to 4. |
Examples |
SENS:CORR:TDR:COLL:DLC:LOAD 1 |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes open (with Thru) measurement, as a part of Loss Compensation sequence. This is used for Single Ended 1 Port only. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<int> |
Port number where open measurement is executed. The range is 1 to 4. |
Examples |
SENS:CORR:TDR:COLL:DLC:OPEN 1 |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command saves the result of the Loss Compensation sequence. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
Examples |
SENS:CORR:TDR:COLL:DLC:SAVE |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes a thru measurement, as a part of Loss Compensation sequence. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<num>,<num> |
Enter the port numbers where the thru is connected. For example, 1,2 indicates that the thru is connected between ports 1 and 2. The range is 1 to 4. |
Examples |
SENS:CORR:TDR:COLL:DLC:THRU 1,2 |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes fixture compensation after ECAL. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
Examples |
SENS:CORR:TDR:COLL:ECAL:FCOM:IMM |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes full calibration using the ECal module. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
Examples |
SENS:CORR:TDR:COLL:ECAL:IMM |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the dielectric constant value. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<value> |
Dielectric constant value. The range is 10m to 100. |
Examples |
SENS:CORR:TDR:DCON 0.01 |
Query Syntax |
SENSe<cnum>:CORRection:TDR:DCONstant? |
Return Type |
Double |
Default |
1 |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes deskew (auto port extension). |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
Examples |
SENS:CORR:TDR:EXT:AUTO:IMM |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the standard for deskew (auto port extension). |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<enum> |
Standard for deskew. Choose from: OPEN - Open termination. SHORt - Short termination. |
Examples |
SENS:CORR:TDR:EXT:AUTO:STAN OPEN |
Query Syntax |
SENSe<cnum>:CORRection:TDR:EXTension:AUTO:STANdard? |
Return Type |
String |
Default |
OPEN |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the reference impedance value. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<value> |
Reference impedance value. The range is 1m to 10M. |
Examples |
SENS:CORR:TDR:RIMP 0.001 |
Query Syntax |
SENSe<cnum>:CORRection:TDR:RIMPedance? |
Return Type |
Double |
Default |
50 |