These commands control the TDR display setup.
DISPlay:TDR EYE | Y | SCALe | AUTO | STATe | RLEVel MEASure | DMEMory | TYPE | X | SCALe | AUTO | RLEVel SCALe | AUTO X | SCALe
|
Click on a red keyword to view the command details.
See Also
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) Turns the continuous auto-scale mode for the eye y-axis ON or OFF. |
|
Parameters |
|
<bool> |
ON or 1 - Turns continuous auto-scale ON. |
Examples |
DISP:TDR:EYE:Y:SCAL:AUTO:STAT ON |
Query Syntax |
DISPlay:TDR:EYE:SCALe:AUTO:STATe? |
Return Type |
Boolean |
Default |
ON |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the value of the y-axis scale per division for eye diagram. |
|
Parameters |
|
<value> |
Value of eye diagram y-axis scale per division. The range is 1E-18 to 5. |
Examples |
DISP:TDR:EYE:Y:SCAL:PDIV 300E-03 |
Query Syntax |
DISPlay:TDR:EYE:Y:SCALe:PDIVision? |
Return Type |
Double |
Default |
0.2 |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the value of the eye diagram y-axis reference line. |
|
Parameters |
|
<value> |
Value of eye diagram y-axis reference line. The range is -5 to +5. |
Examples |
DISP:TDR:EYE:Y:SCAL:RLEV 0.01 |
Query Syntax |
DISPlay:TDR:EYE:Y:SCALe:RLEVel? |
Return Type |
Double |
Default |
0 |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the value of the eye diagram y-axis reference position. |
|
Parameters |
|
<value> |
Value of eye diagram y-axis reference position. The range is 0 to 10. |
Examples |
DISP:TDR:EYE:Y:SCAL:RPOS 10 |
Query Syntax |
DISPlay:TDR:EYE:Y:SCALe:RPOSition? |
Return Type |
Integer |
Default |
4 |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command changes the background color of the screen. |
|
Parameters |
|
<enum> |
Screen background color. Choose from: NORMal - Black background color. INVert - White background color. |
Examples |
DISP:TDR:IMAG NORM |
Query Syntax |
DISPlay:TDR:IMAGe? |
Return Type |
String |
Default |
NORMal |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the display to off, data type, memory type, or data and memory type. |
|
Parameters |
|
<enum> |
Data/memory display. Choose from: OFF - Nothing is displayed on the graph plot. DATA - Data only is displayed on the graph plot. MEMory - Memory only is displayed on the graph plot. DMEMory - Data and Memory are displayed on the graph plot. |
Examples |
DISP:TDR:MEAS1:DMEM:TYPE OFF |
Query Syntax |
DISPlay:TDR:MEASure[1-16]:DMEMory:TYPE? |
Return Type |
String |
Default |
DATA |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes x-axis auto scaling. |
|
Examples |
DISP:TDR:MEAS1:X:SCAL:AUTO display:tdr:measure1:x:scale:auto |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the value of the x-axis scale per division. |
|
Parameters |
|
<value> |
Value of x-axis scale per division. |
Examples |
DISP:TDR:MEAS1:X:SCAL:PDIV 1E-9 |
Query Syntax |
DISPlay:TDR:MEASure[1-16]:X:SCALe:PDIVision? |
Return Type |
Double |
Default |
2n |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the value of the x-axis reference line. |
|
Parameters |
|
<value> |
Value of x-axis reference line. |
Examples |
DISP:TDR:MEAS1:X:SCAL:RLEV 20E-9 |
Query Syntax |
DISPlay:TDR:MEASure[1-16]:X:SCALe:RLEVel? |
Return Type |
Double |
Default |
10n |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) Sets or gets the minimize state. |
|
Parameters |
|
<bool> |
ON or 1 - Turns minimize state ON. |
Examples |
DISP:TDR:MIN:STAT ON |
Query Syntax |
DISPlay:TDR:MINimize:STATe? |
Return Type |
Boolean |
Default |
OFF |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command executes y-axis auto scaling. |
|
Examples |
DISP:TDR:SCAL:AUTO display:tdr:scale:auto |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command selects the view point for waveform analysis either before or after the DUT. |
|
Parameters |
|
<enum> |
X-axis reference position. Choose from: STIMulus - Stimulus view, observation point before DUT. RESPonse - Response view, observation point after DUT. |
Examples |
DISP:TDR:VIEW STIM |
Query Syntax |
DISPlay:TDR:VIEW? |
Return Type |
String |
Default |
RESPonse |
Applicable Models: All with TDR Options (S9x011A/B) (Read-Write) This command sets the x-axis reference position for the time domain measurement. |
|
Parameters |
|
<enum> |
X-axis reference position. Choose from: LEFT - Reference position is the left edge. CENTer - Reference position is center. |
Examples |
DISP:TDR:SCAL:RPOS LEFT |
Query Syntax |
DISPlay:TDR:SCALe:RPOSition? |
Return Type |
String |
Default |
LEFT |