Some applications require the use of IVI-COM to control hardware so that the software SFP does not need to be running in the background.
IVI-COM is the Component Object Model library, maintained by the IVI foundation. Instead of controlling the instrument purely through SCPI commands, IVI-COM behaves more like objects in a .NET environment where dot syntax is used to "navigate" to the desired member function or variable in a hierarchical path.
This solution uses Python and a third-party Python library called Comtypes (see the Comtypes documentation here).
This example was tested working in Python 3.9.6 64-bit and Comtypes library version 1.1.11, 1.1.14 (Comtypes homepage).
IVI drivers are also required, which come with Keysight's IO Libraries. This example uses version 18.2.28014.7.
Installing Comtypes requires pip, which is often installed alongside Python itself. If pip is not installed on your system, see installing pip.
Note: Install the Comtypes library by opening a command prompt and execute:
py -m pip install comtypes
For this example to work with your instrument, you must first change the string variable "VISA_ADDRESS" to match the connection string which refers to your VNA. You can find this string in Keysight Connection Expert:

Any of these three VISA Addresses should work, but the last one is recommended as it is the most human-readable.
Note: If your instrument uses more than one module for the same unit, such as with the P5028A, add both connection strings from Connection Expert to the VISA_ADDRESS string, separated by a semicolon (;).
An example of this is shown in the code block below.
# VNA IVI-COM with Python example code 
	# 
	# Python version 3.9.6 64-bit 
	# Comtypes version 1.1.11 (https://pypi.org/project/comtypes/) 
	# =============================================================== 
	from comtypes.client import GetModule 
	from comtypes.client import CreateObject 
	GetModule("C:\\Program Files\\IVI Foundation\\IVI\\Bin\\AgNA_64.dll") 
	from comtypes.gen import AgNALib 
	def initialize(): 
	    print("Connecting to VNA. Serial Number will be displayed when connection is complete.") 
	          
	    # Change the VISA_ADDRESS string here to match your instrument. 
	    # Find this address in Keysight Connection Expert. 
	    VISA_ADDRESS = 'PXI10::CHASSIS2::SLOT1::FUNC0::INSTR;PXI10::CHASSIS2::SLOT2::FUNC0::INSTR' 
	    initOptions = "QueryInstrStatus=true, Simulate=false, my_VNASetup= Trace=false" 
	    # Syntax: Initialize(VISA_ADDRESS (str), idquery (bool), reset (bool), initOptions (str)) 
	    my_VNA.Initialize(VISA_ADDRESS, False, False, initOptions) 
	def readSerialNumber(): 
	    mySerialNumber = my_VNA.System.SerialNumber 
	    print("\n\nReference SN: ", mySerialNumber) 
	    input("---> Press enter after reviewing serial number.") 
	my_VNA = CreateObject('AgNA.AgNA', interface=AgNALib.IAgNA) 
	initialize() 
	readSerialNumber() 
	# Close connection to VNA reference 
	print("\n\nClosing connection to VNA.") 
	my_VNA.Close() 
	print("\nConnection to VNA closed.")