This example program does the following:
Sets up measurement for either PNOP or PSAT marker search
Sets parameters for search
Reads a parameter for each
See PNOP and PSAT SCPI commands.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as SearchMkr.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
Dim app Set app = CreateObject("AgilentPNA835X.Application") Dim scpi set scpi = app.ScpiStringParser scpi.Execute ("SYST:FPReset") ' View Power Out vs Power In ' Create and turn on window/channel 1 scpi.Execute ("DISPlay:WINDow1:STATE ON") 'Define a measurement name, parameter scpi.Execute ("CALCulate1:PARameter:DEFine:EXT 'MyMeas','B,1'") 'Associate ("FEED") the measurement name ('MyMeas') to WINDow (1) scpi.Execute ("DISPlay:WINDow1:TRACe1:FEED 'MyMeas'") scpi.Execute ("CALCulate1:PARameter:SELect 'MyMeas'") 'perform power sweep scpi.Execute ("SENSe1:SWEep:TYPE POWer") scpi.Execute ("SOURce1:POWer:STARt -5") scpi.Execute ("SOURce1:POWer:STOP 0") '-------------------- 'Choose marker search resp=Msgbox ("PNOP (yes) or PSAT (no)" , 4, "PNA Marker Search Demo") if resp=6 then PNOP1() Else PSAT1() End If '-------------------- 'PSAT marker search Sub PSAT1() scpi.Execute ("CALCulate1:MARKer:PSATuration:BACKoff 2") 'Read PSAT Parameter dim answer answer=scpi.Execute ("CALCulate1:MARKer:PSATuration:GAIN?") wscript.echo("Gain Sat: "& answer) End Sub '-------------------- 'PNOP marker search Sub PNOP1() scpi.Execute ("CALCulate1:MARKer:PNOP:BACKoff 2") scpi.Execute ("CALCulate1:MARKer:PNOP:POFFset 1") 'Read PNOP Parameter dim answer answer=scpi.Execute ("CALCulate1:MARKer:PNOP:GAIN?") wscript.echo("PNOP Gain: "& answer) End Sub  |