This VBScript program configures and displays Phase Sweep measurements.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as RxLev.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
'Assume port 1 is connected to port 3 Set pna = CreateObject("AgilentPNA835x.Application") Set SCPI = PNA.ScpiStringParser 'Create 3 trace S33, R3/C(amp),R3/C(phase) SCPI.Parse("SYST:FPR") SCPI.Parse("DISP:WIND:STATE ON") SCPI.Parse("CALC:PAR:DEF 'MyMeas1',S33") SCPI.Parse("DISP:WIND1:TRAC1:FEED 'MyMeas1'") SCPI.Parse("CALC:PAR:SEL 'MyMeas1'") SCPI.Parse("CALC:FORM SMIT") SCPI.Parse("CALC:PAR:DEF 'MyMeas2',R3C,3") SCPI.Parse("DISP:WIND1:TRAC2:FEED 'MyMeas2'") SCPI.Parse("CALC:PAR:SEL 'MyMeas2'") SCPI.Parse("CALC:FORM MLOG") SCPI.Parse("CALC:PAR:DEF 'MyMeas3',R3C,3") SCPI.Parse("DISP:WIND1:TRAC3:FEED 'MyMeas3'") SCPI.Parse("CALC:PAR:SEL 'MyMeas3'") SCPI.Parse("CALC:FORM PHAS") SCPI.Parse("SENS:SWE:TYPE PHAS") 'turn on 3 and 1 SCPI.Parse("SOUR:POW1:MODE ON") SCPI.Parse("SOUR:POW3:MODE ON") 'set port3's control parameter to R3/C SCPI.Parse("SOUR:PHAS3:PAR 'R3/C'") 'Set port3 to PAR mode SCPI.Parse("SOUR:PHAS3:PAR:MODE PAR") SCPI.Parse("SOUR:PHAS3:PAR:PORT 1") SCPI.Parse("SOUR:PHAS3:POFF:FIX 3") SCPI.Parse("SOUR:PHAS3:STAR 0") SCPI.Parse("SOUR:PHAS3:STOP 180")  |