This example program demonstrates how to perform a simulated eye diagram written in Excel VBA (VISA-COM).
See Other SCPI Example Programs
| Dim rm As VisaComLib.ResourceManager Dim vna As VisaComLib.FormattedIO488 Sub Message(msg As String) Dim NumDmy As Integer 'Syncronize to VNA vna.WriteString "*OPC?" NumDmy = vna.ReadNumber 'Write Message MsgBox msg, vbOKOnly End Sub Sub SimEyeDiagram() On Error GoTo errorhandler Set rm = New VisaComLib.ResourceManager Set vna = New VisaComLib.FormattedIO488 
 ' Set your VNA address Set vna.IO = rm.Open("TCPIP0::K-N5232B-40046::hislip0::INSTR") vna.IO.Timeout = 90000 
 ' Clear Excel Sheet Cells Range("A1:F22").ClearContents 
 With vna Dim i As Integer 
 ' Set DUT Topology to Differential 2-Port .WriteString ":CALC:TDR:DEV DIF2" ' Execute Deskew using TDR Setup Wizard .WriteString ":DISP:TDR:MIN:STAT OFF" Message "[Deskew]" + vbCrLf + _ "1. Press 'TDR Setup Wizard' on TDR GUI." + vbCrLf + _ "2. Select 'Deskew' and complete the wizard with 'Finish' button." + vbCrLf + _ "3. Confirm 'TDR [Deskew]' indicator appears on VNA status line." + vbCrLf + _ "4. Press OK button to continue." 
 ' Minimize TDR GUI .WriteString ":DISP:TDR:MIN:STAT ON" 
 ' Set Rise Time .WriteString "CALC:PAR:COUN?" 'Get number of traces For i = 1 To .ReadNumber .WriteString ":CALC:TDR:MEAS" + CStr(i) + ":TIME:STEP:RTIM:THR T2_8" 'Threshold .WriteString ":CALC:TDR:MEAS" + CStr(i) + ":TIME:STEP:RTIM 50e-12" 'Rise Time Next i 
 ' Set Bit Pattern Parameters .WriteString ":CALC:TDR:EYE:INP:BPAT:TYPE PRBS" 'Type .WriteString ":CALC:TDR:EYE:INP:BPAT:LENG 7" 'Length .WriteString ":CALC:TDR:EYE:INP:OLEV 200e-3" 'One Level .WriteString ":CALC:TDR:EYE:INP:DRAT 1e9" 'Data Rate ' Set Rise Time/Threshold .WriteString ":CALC:TDR:EYE:INP:RTIM:DATA 50e-12" .WriteString ":CALC:TDR:EYE:INP:RTIM:THR T2_8" ' Activate Trace 5 (Tdd21) .WriteString ":CALC:PAR:MNUM:SEL 5" ' Execute Draw Eye Message "Connect DUT to cables." + vbCrLf + "Press OK to draw Eye diagram." .WriteString ":CALC:TDR:EYE:STAT ON" .WriteString ":CALC:TDR:EYE:EXEC" ' Read Eye Results Cells(3, 4) = "Eye Results" Dim Labels() As Variant Labels = Array("Min. Value", "Max. Value", "Level Zero", "Level One", "Level Mean", "Amplitude", "Height", "(Reserved)", "Width", "Opening Factor", _ "Signal/Noise", "Duty Cycle Dist", "Duty Cycle Dist(%)", "Rise Time", "Fall Time", "Jitter p-p", "Jitter RMS", "Crossing %") Dim EyeResult() As Double .WriteString ":CALC:TDR:EYE:RES:DATA?" EyeResult() = .ReadList(ASCIIType_R8, ",") For i = 0 To 17 'Number of results = 18 Cells(i + 5, 4) = Labels(i) Cells(i + 5, 6) = EyeResult(i) Next i 
 ' Restore TDR GUI .WriteString ":DISP:TDR:MIN:STAT OFF" Message "Finished Simulated Eye Diagram." End With 
 vna.IO.Close Exit Sub errorhandler: MsgBox Err.Description, vbExclamation, "Error Occurred", Err.HelpFile, Err.HelpContext End Sub |