This example program demonstrates how to perform TDR/TDT setup written in Excel VBA (VISA-COM).
See Other SCPI Example Programs
Dim rm As VisaComLib.ResourceManager Dim vna As VisaComLib.FormattedIO488 Sub Message(msg As String) Dim NumDmy As Integer 'Syncronize to VNA vna.WriteString "*OPC?" NumDmy = vna.ReadNumber 'Write Message MsgBox msg, vbOKOnly End Sub Sub TDRTDTMeasure() On Error GoTo errorhandler Set rm = New VisaComLib.ResourceManager Set vna = New VisaComLib.FormattedIO488
' Set VNA Address Set vna.IO = rm.Open("TCPIP0::K-N5232B-40046::hislip0::INSTR") vna.IO.Timeout = 90000
' Clear Excel Sheet Cells Range("D5:F5").ClearContents
With vna Dim i As Integer
' Set DUT Topology to Differential 2-Port .WriteString ":CALC:TDR:DEV DIF2"
' Desckew and Loss Compensation ' Desckew .WriteString ":SENSe:CORR:TDR:EXTension:AUTO:IMMediate", True .WriteString "*OPC?", True NumDmy = .ReadNumber ' MsgBox "Connect thru between ports 1 and 3.", vbOKOnly .WriteString ":SENS:CORR:TDR:COLL:DLC:THRU 1,3", True .WriteString "*OPC?", True NumDmy = .ReadNumber
MsgBox "Connect thru between ports 2 and 4.", vbOKOnly .WriteString ":SENS:CORR:TDR:COLL:DLC:THRU 2,4", True .WriteString "*OPC?", True NumDmy = .ReadNumber
' Loss Compensation, thru MsgBox "Connect a Load to the ports 1,2,3,4.", vbOKOnly .WriteString ":SENS:CORR:TDR:COLL:DLC:LOAD 1", True .WriteString "*OPC?", True NumDmy = .ReadNumbe .WriteString ":SENS:CORR:TDR:COLL:DLC:LOAD 2", True .WriteString "*OPC?", True NumDmy = .ReadNumber .WriteString ":SENS:CORR:TDR:COLL:DLC:LOAD 3", True .WriteString "*OPC?", True NumDmy = .ReadNumber .WriteString ":SENS:CORR:TDR:COLL:DLC:LOAD 4", True .WriteString "*OPC?", True NumDmy = .ReadNumber
' Save the data to finish the Deskew and Loss Compensation .WriteString ":SENS:CORR:TDR:COLL:DLC:SAVE", True .WriteString "*OPC?", True NumDmy = .ReadNumber
' Set Rise Time .WriteString "CALC:PAR:COUN?" 'Get number of traces For i = 1 To .ReadNumber .WriteString ":CALC:TDR:MEAS" + CStr(i) + ":TIME:STEP:RTIM:THR T2_8" 'Threshold .WriteString ":CALC:TDR:MEAS" + CStr(i) + ":TIME:STEP:RTIM 50e-12" 'Rise Time Next i
' Measure Message "Connect DUT to cables." + vbCrLf + "Press OK to execute measurement." .WriteString ":SENS:TDR:SWE:SING;*OPC?" NumDmy = .ReadNumber ' Auto Scale for all traces .WriteString ":DISP:TDR:SCAL:AUTO"
' Read Rise Time of Tr 5 (Tdd21) Cells(5, 4) = "Rise Time" .WriteString ":CALC:TDR:MEAS5:TTIM:STAT ON" .WriteString ":CALC:TDR:MEAS5:TTIM:THR T2_8" .WriteString ":CALC:TDR:MEAS5:TTIM:DATA?" Cells(5, 6) = .ReadNumber
' Restore TDR GUI .WriteString ":DISP:TDR:MIN:STAT OFF" Message "Finished TDT/TDT Measurement." End With
vna.IO.Close Exit Sub errorhandler: MsgBox Err.Description, vbExclamation, "Error Occurred", Err.HelpFile, Err.HelpContext End Sub |
|