This example shows how to use an existing Source Power Cal instead of the power cal that is performed during an SMC calibration. To run this program without modification, you need the following:
A Mixer setup file saved on the VNA: C:\Program Files(x86)\Keysight\Network Analyzer\Documents\Mixer\MyMixer.mxr.
If the mixer file uses an external LO source, it must also be attached and configured.
An ECAL module that covers the frequency range of the measurement.
An SMC cal set named "SMC_CAL". This is the cal set that source power correction data will be imported from. The input and output frequency ranges of the cal set must cover the corresponding ranges used during calibration, or guided cal initialization will fail.
If you attempt to import power cal data from an SMC calset that uses different ports than the ones currently in use, the message “The necessary calibration standards were not found.” will appear.
If the imported Cal Set does not cover the frequency range of the current cal, the message “Interpolation target is out of range. Cannot interpolate.” will appear.
Sens:Corr:Coll:Guid:SMC commands
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save on the VNA hard drive as SMC.vbs. Learn how to setup and run the macro.
Dim app Dim scpi ' Create / Get the VNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser '---Create a Scalar Mixer Forward Measurement 'First, delete all measurements on the channel scpi.Parse "CALC:PAR:DEL:ALL" 'Create a forward scalar mixer measurement and configure it in 'channel 1. The first parameter is a unique 'identifying string (specified by the user) to allow subsequent 'commands to be directed at this specific measurement. scpi.Parse "CALC:CUST:DEF 'My SC21', 'Scalar Mixer/Converter', 'SC21'" 'Setup the new measurement as the 2nd trace in the active window scpi.Parse "DISP:WIND:TRAC2:FEED 'My SC21'" 'Make the new trace the active measurement scpi.Parse "CALC:PAR:SEL 'My SC21'" 'The parameters of the mixer measurement can now be configured. 'This can be done by either using the individual SENS:MIX commands 'for each of the parameters or by loading a mixer setup file. This 'example loads a mixer setup file. The path name 'for the mixer file may be loaded from other mapped drives scpi.Parse "SENS:MIXer:Load ""C:\Program Files(x86)\Keysight\Network Analyzer\Documents\Mixer\MyMixer.mxr"""
'--------------Perform A Scalar Mixer Calibration---------------------- 'Specify the connector types and the cal kits for each of the ports. scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT1:SEL ""APC 3.5 male""" scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT2:SEL ""APC 3.5 female""" scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT1:SEL ""N4691-60004 ECal""" scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT2:SEL ""N4691-60004 ECal""" 'Import power cal data from the existing SMC calset "MySMC" scpi.Parse "SENS:CORR:COLL:GUID:SMC:IMP ""SMC_CAL"",""POWER_STEP""" 'Specify the thru measurement method. This applies to both ECal 'and mechanical calibrations. 'Always send the init command before the Thru method command scpi.Parse "SENS:CORR:COLL:GUID:INIT" scpi.Parse "SENS:CORR:COLL:GUID:PATH:TMET 1,2,""DEFINED THRU""" 'Omit the isolation part of the 2-port cal (default behavior). scpi.Parse "SENS:CORR:COLL:GUID:ISOL NONE" 'Turn on auto orientation for the ECal (default behavior). scpi.Parse "SENS:CORR:PREF:ECAL:ORI ON" 'Initialize an SMC guided calibration. scpi.Parse "SENS:CORR:COLL:GUID:INIT" 'Tell the wizard to generate and report the number of steps in this cal. Dim steps Dim desc 'Determine the number of steps required to complete the calibration. steps = scpi.Parse ("SENS:CORR:COLL:GUID:STEP?") For i = 1 To steps 'Display the prompt for each step desc = scpi.Parse ("SENS:CORR:COLL:GUID:DESC? " & CStr(i)) MsgBox (desc) 'Perform the measurement for each step scpi.Parse "SENS:CORR:COLL:GUID:ACQ STAN" & CStr(i) Next Dim calset 'Finish the cal and save the calset calset = scpi.Parse ("SENS:CORR:COLL:GUID:SAVE OFF") Msgbox ("SMC cal saved to cal register") |