Click System > Help > About NA... to learn the capabilities of your analyzer.

Model number
Frequency range
Serial number
Options (Learn how to install software options)
Application Code (firmware) Version
Solid State Drive Version
System CPU Version - Learn more
DSP (Digital Signal Processor.) Version. Contact Keysight to upgrade the DSP.
Computer Name - Learn more. This is also reported on the LAN Status / LXI Compliance dialog.

Model number (see list of models)
Options (Learn how to install software options)
If "Ignored" is labeled on the application model number, the application is not supported.
PXI Modules: Select the required module to show the information in the window below
Product number, S/N, Host ID
Calibration Date
Hardware options
Computer Name - Full computer name of the Embedded Controller when used.