When testing devices remotely using SCPI, the following techniques can be used to transfer data quickly between the analyzer and remote computer, helping you achieve the best measurement throughput.
Use single sweep (trigger) mode to ensure that a measurement is complete before starting a data transfer.
Transfer the minimum amount of data needed. For example, a trace with a few points, using segment sweep rather than a full trace with many linearly spaced points. Also, use markers instead of trace transfers.
Choose the REAL data format to provide the fastest transfer speed when using SCPI programs for automated applications.
Use SCPI over LAN for applications that are automated with SCPI programs.
Use Shared Memory Data Transfer. Learn how.