Firmware Update (Core Software Update)


VNA firmware updates are available to you at no cost in a self-extracting Install Shield file. The update includes the VNA application, Online help, and Service Utilities.

To manually check the version of firmware on the VNA, click System > Help > About NA....

Note: After a firmware update...

  • Custom Cal Kits must be imported. Learn more

  • If a different desktop icon named "Network Analyzer" exists, the shortcut to the VNA application will assume the same icon. Right-click on the desktop, then click Refresh.

Other Support Topics

Updating firmware

  1. Download the latest firmware from http://www.keysight.com/find/na  

  2. Terminate the VNA application by pressing System > Main > Exit.

  3. Transfer the file from your PC to your VNA using LAN or USB Pen drive.

  4. Double-click the file on the VNA and follow the instruction.