Pathwave Calibration Advisor (PCA)

Pathwave Calibration Advisor (PCA) is a tool that that monitors the calibration status of instruments and notifies users when a factory calibration is approaching its due date or has expired. It helps users maintain calibration compliance by providing timely reminders.

 

How PCA works

The Pathwave Calibration Advisor (PCA) relies on calibration information stored in the instrument to monitor calibration status and notify users when calibration is due.

This process provides increased visibility into calibration status, simplifies calibration management, and helps reduce the risk of operating instruments with expired calibrations.

 

Supported Models

This following VNA products support Pathwave Calibration Advisor (PCA).

Type

Model Name

PCA Type

PXIe

M980xA 

M983xA 

PCA 2.x 

Streamline

P50xxA 

P50xxB/BQ/M 

P937xB 

P938xB 

PCA 2.x 

Benchtop

PNA series (N52xxB, NA52xxA)

ENA8 series (E5080B, E5081A) 

SSA-X (E505xA)

PCA 1.x 

PXIe

 

M937xA

Not supported

Streamline

P937xA

Not supported

Simulator

All models 

Not supported

 

Installation

The VNA installer automatically installs and configures all PCA components. No additional user action is required.

 

How to open Pathwave Calibration Advisor (PCA) Status dialog

How to launch Pathwave Calibration Advisor (PCA)

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press System > Service> VNA Cal Status....

 

  1. Click on Utility.

  2. Select SystemService then VNA Cal Status...

Programming Commands

 

PCA 1.x Dialog

 

PCA 2.x Dialog

Cal Due Notification

When the VNA firmware starts, a notification popup is displayed if a module calibration has expired or reaching to the due date.

 

For information on how to set up the PathWave Calibration Advisor, click on in the top-right part of the dialog to access the PathWave Calibration Advisor Help.