Last updated: 2010-03-31
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Stops all measurements that are active. If the trigger arm is set to single, the measurements will go to the idle state. If the trigger arm is set to continuous, the measurements will re-arm and initiate again. |
|
Setting |
No setting |
|
Query |
No Query |
|
*RST Setting |
None |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"ABORt" |
|
Function |
Stops the selected measurement if it is active. If the trigger arm is set to single, the measurements will go to the idle state. If the trigger arm is set to continuous the measurements will re-arm and initiate again. |
|
Setting |
|
|
Query |
No Query |
|
*RST Setting |
None |
|
Requirements |
Test Application Revision: A.01.00 and above Test Application Revision: A.03.00 and above, added TOLP, TBLerror and THBLerror. Test Application Revision: A.04.00 and above, added TOOSynch, TFDT, THCQuality. Test Application Revision: A.08.00 and above, added DEHich and DEAGch. |
|
Programming Example |
"ABORt:TCPower" |