Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the primary common control physical channel's initial power. The setting can be set in active cell operating mode only when the call status is Idle, or in other operating modes. |
|
Setting |
Range: +6 to +43 dBm |
|
Query |
Range: 6 to 43 |
|
*RST Setting |
24 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"CALL:CCPChannel:PRIMary:BLEVel 24" |