Show 

Home > Call Processing > Call Parms > Call Drop Timer

Call Drop Timer

Last updated: 2010-03-31

Description

The call drop timer can be enabled (turned on) or disabled (turned off).

Once a call is established, if the call drop timer is enabled, the call drop timer is started.

When the call drop timer is turned on, if the test set is unable to synchronize with the midamble in the uplink DPCH for a period of 500 ms, the call drop timer expires and the test set drops the call connection with an error message.

Related Topics

GPIB Commands: CALL:CONNected:DROP:TIMer[:STATe][:SELected]