DISPlay Subsystem

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

DISPlay:BRIGhtness

Function

Sets/queries the test set's display brightness.

Setting

Range: MEDium | HIGH

Query

Range: MED | HIGH

*RST Setting

HIGH

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"DISPlay:BRIGhtness MEDium"

DISPlay:MODE

Function

Sets/queries the test set's display mode.

Setting

Range: FAST | TRACK

Query

Range: FAST | TRAC

*RST Setting

TRACK

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"DISPlay:MODE FAST"

DISPlay:MESSage:MASKable:STATe

Function

Blocks maskable messages from appearing on the test set display screen but not from the Message Log.

Maskable messages are reported to the Message Log in either state.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

On

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"DISPlay:MESSage:MASKable:STATe OFF"