RFGenerator Subsystem
Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
Function |
Sets/queries the RF output port destination: RF IN/OUT (IO) or RF OUT ONLY (OUT). |
Setting |
Range: IO|OUT |
Query |
Range: IO|OUT |
*RST Setting |
IO |
Requirements |
Test Application Revision: A.01.00 and above |
Programming Example |
"RFGenerator:OUTPut OUT" |