Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions.
For the measurement, see Adjacent Channel Leakage Ratio (ACLR) Measurement.
|
Function |
Sets/queries the trigger arm state for the adjacent channel leakage measurement. The trigger arm state determines whether the adjacent channel leakage measurement will be made once then stop (0|OFF (single)), or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)). |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:CONTinuous OFF" |
|
Function |
The setting form of this command performs two functions: (1) sets the number of adjacent channel leakage measurements to be made in a multi-measurement, and (2) sets the multi-measurement STATe command to 1 (on). The query form returns the number of adjacent channel leakage multi-measurements to be made when multi-measurement state is ON. |
|
Setting |
Range: 1 to 999 |
|
Query |
Range: 1 to 999 |
|
*RST Setting |
Off (10 when STATe = On) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:COUNt:SNUMber 5" |
|
Function |
Sets/queries the number of adjacent channel leakage measurements to be made when the multi-measurement state is ON. |
|
Setting |
Range: 1 to 999 |
|
Query |
Range: 1 to 999 |
|
*RST Setting |
10 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:COUNt:NUMBer 5" |
|
Function |
Sets/queries the adjacent channel leakage multi-measurement state. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:COUNt:STATe ON" |
|
Function |
Sets/queries the Adjacent (±1.6MHz) and the Alternate (±3.2MHz) limit for the ACLR measurement. |
|
Setting |
Range: -80 to +10 dBc Resolution: 0.01 |
|
Query |
Same as setting |
|
*RST Setting |
-33, -43 ( adjacent limit, alternate limit) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:LIMit -33, -43" |
|
Function |
Sets/queries the value of Manual Power Range Offset. |
|
Setting |
Range:-25dB to 25dB Resolution: 0.01 dB Unit: dB |
|
Query |
Range:-25dB to 25dB |
|
*RST Setting |
0.00dB |
|
Requirements |
Test Application Revision: A.06.00 and above |
|
Programming Example |
"SETup:TACLeakage:POWer:RANGe:OFFSet:MANual 6dB" |
|
Function |
The setting form of this command performs two functions: (1) sets the adjacent channel leakage measurement's timeout value, and (2) sets the adjacent channel leakage measurement's timeout STATe to 1 (on). The query form returns the adjacent channel leakage measurement's timeout value. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 seconds, off |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:TIMeout:STIMe 5 S" |
|
Function |
Sets/queries the adjacent channel leakage measurement's timeout state. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:TIMeout:STATe ON" |
|
Function |
Sets/queries the adjacent channel leakage measurement's timeout setting to be used when the timeout state is set to ON. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 seconds |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:TIMeout:TIME 5 S" |
|
Function |
Sets/queries the adjacent channel leakage measurement's Trigger Delay setting. This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame. For example, a 1.333 ms delay would cause the trigger to wait until after the first two timeslots have elapsed. |
|
Setting |
Range: -10 to 10 ms Resolution: 0.1 us Unit: S | MS | US | NS |
|
Query |
Same as setting |
|
*RST Setting |
0 seconds |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:TRIGger:DELay 1 MS" |
|
Function |
Sets/queries the adjacent channel leakage measurement's Trigger Source . |
|
Setting |
Range: AUTO | IMMediate | RISE | EXTernal | PROTocol |
|
Query |
Range: AUTO | IMM | RISE | EXT |PROT |
|
*RST Setting |
AUTO |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SETup:TACLeakage:TRIGger:SOURce AUTO" |
|
Function |
Sets/queries which uplink time slot to be measured. |
|
Setting |
Range: TS1 | TS2 | TS3 |TS4 |
|
Query |
Same as setting |
|
*RST Setting |
TS1 |
|
Requirements |
Test Application Revision: A.06.00 and above |
|
Programming Example |
"SETup:TACLeakage:TSLot:MEASure TS1" |