Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
For the measurement, see Occupied Bandwidth (OBW) Measurement.
|
Function |
The setting form of this command performs two functions: (1) sets the number of occupied bandwidth measurement to be made in a multi-measurement, and (2) sets the multi-measurement state to 1 (ON). The query form returns the number of occupied bandwidth multi-measurements to be made when multi-measurement state is ON. |
|
Setting |
Range: 1 to 999 |
|
Query |
Range: 1 to 999 |
|
*RST Setting |
OFF (10 when STATe = ON) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETUP:TOBWidth:COUNT 5" |
|
Function |
Sets/queries the number of occupied bandwidth measurement to be made when the multi-measurement state is ON. |
|
Setting |
Range: 1 to 999 |
|
Query |
Range: 1 to 999 |
|
*RST Setting |
10 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETUP:TOBWidth:COUNT:NUMBER 5" |
|
Function |
Sets/queries the occupied bandwidth multi-measurement state. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (OFF) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TOBWidth:COUNt:STATe ON" |
|
Function |
Sets/queries the trigger arm state for the occupied bandwidth measurement. The trigger arm state determines whether the occupied bandwidth measurement will be made once then stop (0|OFF (single)), or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)). |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (OFF) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TOBWidth:CONTinuous OFF" |
|
Function |
Sets/queries the percentage of total power used in the occupied bandwidth measurement. The total power is measured in a 4.8 MHz bandwidth. |
|
Setting |
Range: 70.0 to 99.0 percent Resolution: 0.01 percent |
|
Query |
Same as setting |
|
*RST Setting |
99 |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TOBWidth:PERCent 99" |
|
Function |
The setting form of this command performs two functions: (1) sets the occupied bandwidth measurement's timeout value, and (2) sets the occupied bandwidth measurement's timeout state to 1 (on). The query form returns the occupied bandwidth measurement's timeout value. |
|
Setting |
Range: 0.1 to 999.9 seconds Unit: S | MS | US | NS |
|
Query |
Same as setting |
|
*RST Setting |
10 s, on |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TOBWidth:TIMeout:STIMe 5S" |
|
Function |
Sets/Queries the occupied bandwidth measurement's timeout state. |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0(OFF) |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TOBWidth:TIMeout:STATe ON" |
|
Function |
Sets/queries the occupied bandwidth measurement's timeout setting to be used when the timeout state is set to ON.. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second Unit: S | MS | US | NS |
|
Query |
Range: 0.1 to 999.9 |
|
*RST Setting |
10 s |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETup:TOBWidth:TIMeout:TIME 10S" |
|
Function |
Sets/queries the occupied bandwidth measurement's trigger delay setting. This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame. |
|
Setting |
Range: -10 to 10 ms Resolution: 0.1 us Unit: S | MS | US | NS |
|
Query |
Same as setting |
|
*RST Setting |
0 ms |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETUP:TOBWidth:TRIGGER:DELAY 0MS" |
|
Function |
Sets/queries the occupied bandwidth measurement's trigger source. |
|
Setting |
Range: AUTO | IMMediate | RISE | EXTernal | PROTocol |
|
Query |
Range: AUTO | IMM | RISE | EXT | PROT |
|
*RST Setting |
AUTO |
|
Requirements |
Test Application Revision: A.02.00 and above |
|
Programming Example |
"SETUP:TOBWidth:TRIGGER:SOURCE AUTO" |