SYSTem:Kit

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

SYSTem:KIT:UPGRade[:NUMBers]?

Function

Queries the numbers of the E5515 kits hardware upgrades.

Query

Range: Any string with 256 characters

*RST Setting

9.91E+37

Requirements

Test Application Revision: A.08.00 and above

Programming Example

OUTPUT 714;"SYSTEM:KIT:UPGRADE?" !