Trig Output Setup

Last updated: 2010-05-13

Description

The test set provides a 5 V, 25 us pulse at the TRIG OUT rear panel connector for triggering other test equipment from the test set.

This pulse is generated according to the Trigger Output Setup setting:

When Trigger Output Setup is set to System Frame Clock, pulses are generated with a period of 10 ms, in alignment with the first symbol period of each frame.

When Trigger Output Setup is set to Measurement Generated, pulses are generated with a period determined by the measurement that is currently running.

Related Topics

GPIB Commands: CALL:TRIGger