Application Selection

Last updated: 2010-03-31

Description

Different radio formats (such as TD-SCDMA, GSM,  CDMA 2000 or TIA/EIA 136) can be tested when applications are purchased from Keysight Technologies. Different revisions of the applications in your test set provide different capabilities.  The test set allows you to switch between different applications, and once you select a revision the revision does not change unless you select another revision. Switching to another application takes about one minute.

To perform Application Selection, press the SYSTEM CONFIG key, followed by the Application Selection key.

License Status

Revisions are shown with their license status. After the revision number is a letter. That letter indicates the revision license status; Licensed "L", Not Licensed "N", or Unknown "U".

"L"- This revision of application appears to have a License. The application may have been developed before licensing and therefore needs no license.

"N" - This application does not appear to have a license.

"P" - Some Part of the application does not appear to have a license.

"U" - This application has Unknown license status.

Related Topics

GPIB Commands: SYSTem:APPLication